cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H563VIT6 DAC1 Output Unexpected

mccabehm
Senior

Driving DAC1 channel 1 with

 

 

 

 

HAL_DAC_Start(&hdac1, DAC_CHANNEL_1); ... while (1) { HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 4095UL); HAL_Delay(100UL); HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 0UL); HAL_Delay(100UL); }

 

 

 

 

to generate 5 Hz, 50% duty cycle, 0 - 2.5v. Amplitude as expected but frequency varies from 1 - 4s and duty cycle varies from 20 - 80%: not expected. DAC1 configured like

mccabehm_1-1738710940044.png

DAC1 clocked at 65 MHz. When I step into HAL_DAC_SetValue() I see where the 0 - 4095 value is written to data register (12-bit, right-aligned). But sometimes after writing 4095 the output pin reads zero; and sometimes after writing zero the output pin reads 2.5v. I can't explain why this happens. DAC Instance following write looks like

mccabehm_2-1738711213554.png

I am the only writer on the data register.

1 ACCEPTED SOLUTION

Accepted Solutions
mccabehm
Senior
9 REPLIES 9
mccabehm
Senior

Custom board. I lifted the op amp pin connected to PA4 (DAC1 channel 1). Same behavior. This isolates the problem to the MCU and DAC peripheral.

mccabehm
Senior

Using same custom board, I ran an old project capable of generating the desired waveform. It works; desired waveform generated.

The new project (cannot generate desired waveform) used STM32CubeMX 6.13 and STM32Cube FW_H5 V1.4.0.

The old project (waveform good) used STM32CubeMX 6.12 and STM32Cube FW_H5 V1.3.0. I migrated the old project to STM32CubeMX 6.13 and STM32Cube FW_H5 V1.4.0. Now the old project which used to work -- fails. It manifests the same weird DAC behavior as the new project.

The code generated from the IOC file is identical. So the only difference is FW_H5 V1.4.0 vs FW_H5 V1.3.0.

How do I revert the project to STM32CubeMX 6.12 and FW_H5 V1.3.0?

waclawek.jan
Super User

What is the reference, VREF+?

JW

2.5v

waclawek.jan
Super User

Did you measure it?

JW

Yes. 2.57 to be exact. Stable.

mccabehm
Senior

I conclude: either the following code is wrong for running the DAC

 

HAL_DAC_Start(&hdac1, DAC_CHANNEL_1); ... while (1) { HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 4095UL); HAL_Delay(100UL); HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 0UL); HAL_Delay(100UL); }

 

or there's something wrong with migrating to STM32CubeMX 6.13 and STM32Cube FW_H5 V1.4.0 for H563.

If the migration is the problem, I need to revert a project from H5 V1.4.0 to V1.3.0. How to do that easily? Or do I remove H5 V1.4.0 from the repository and then re-create a project to grab the latest firmware version?

mccabehm
Senior

Comparing stm32h5xx_hal_msp.c from the "good" project and the "bad" project I see the "good" project has the following, which is absent from the "bad" project

RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0}; if(hdac->Instance==DAC1) { /* USER CODE BEGIN DAC1_MspInit 0 */ /* USER CODE END DAC1_MspInit 0 */ /** Initializes the peripherals clock */ PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DAC; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) { Error_Handler(); }

 Adding the above code to the "bad" project's stm32h5xx_hal_msp.c fixes the problem.

What needs to change in the "bad" project's IOC file to add the above code to stm32h5xx_hal_msp.c? There is nothing obvious in the GUI representations of the IOC files to explain the difference.

I am attaching IOC files from "good" and "bad" projects. I don't see anything in a diff of the 2 files to explain the missing code.

The stm32h5xx_hal_msp.c for the "good" project was generated with STM32CubeMX v6.12.0. The stm32h5xx_hal_msp.c for the "bad" project was generated with STM32CubeMX v6.13.0. At this point I am suspicious of MX 6.13.0.

mccabehm
Senior