cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H563 Debug mode stopped working

redsire
Associate II

Hello,

While debugging STM32H5 SPI2 (slave and master) in receive mode, the debug suddenly stopped and somehow I can't work in debug again.

1 ACCEPTED SOLUTION

Accepted Solutions
redsire
Associate II

Hello,

 

I tried another debugger (J-Link) and it worked, then I tried connecting with ST-Link V2 again and it worked too.

Thanks to everyone who tried to help.

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

You're going to need to give a lot more detail for anyone to be able to help!

See the Posting Tips:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 


@redsire wrote:

the debug suddenly stopped 


What debugger (software & hardware) were you using?

What is your target hardware?

What, exactly, were you doing before it "stopped"?

What, exactly, happened?  Were there error messages? Was there smoke?

 


@redsire wrote:

somehow I can't work in debug again.


So what, exactly, does happen when you try to debug?

Can you debug any other target(s)? Can you load other firmware?

Have you reset and/or power-cycled the target before trying again?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

> You're going to need to give a lot more detail for anyone to be able to help!

Correct.
"Doesn't work anymore" contains nothing to really work with.


I would suspect a core lock-up, due to a faulty exception handler.

I'm sorry its my mistake, i should to give a lot more detail.

What debugger (software & hardware) were you using? I'm using IAR Embedded Workbench IDE 9.40 and ST-LINK V2

What is your target hardware? My target hardware is NXP MKM34Z256VLL7. I tried ST as master and also ST as slave but I got the same problem in receive mode in both.

What, exactly, were you doing before it "stopped"? In the last one, I put the code 'DATA_TransferCompleteRx();' in the comment line of the DMA interrupt and tried to restart the debugger. Details below:

 

 

void DATA_TransferCompleteRx(void) { LL_SPI_DisableDMAReq_RX(DATA_SPI); LL_DMA_DisableChannel(GPDMA1, LL_DMA_CHANNEL_0); LL_SPI_Disable(DATA_SPI); if(LL_DMA_IsActiveFlag_TC(GPDMA1, LL_DMA_CHANNEL_0)) { LL_DMA_ClearFlag_TC(GPDMA1, LL_DMA_CHANNEL_0); } LL_DMA_DisableIT_TC(GPDMA1, LL_DMA_CHANNEL_0); //LL_SPI_EnableIT_EOT(DATA_SPI); gRxCompleted = true; LL_SPI_Enable(DATA_SPI); for(uint8_t i = 0; i < 4; i++) { DATA_Send(gTxBuffer[i]); } }

 

 

What, exactly, happened?  Were there error messages? Was there smoke? The error massage: "Target is running, Failed to stop the target. Maybe the target needs to be reset. Try again?" 

So what, exactly, does happen when you try to debug? If i try again debug ?? It freezes in busy mode until I press the cancel button and when i press cancel the same massage coming: "Target is running, Failed to stop the target. Maybe the target needs to be reset. Try again?"

Can you debug any other target(s)? Can you load other firmware? Yes, i can debug MKM or another ST mcu in another project.

Have you reset and/or power-cycled the target before trying again? I did try pulling the BOOT pin to HIGH.

I don't know the H5, to put this upfront. Although I think this is not especially significant.

Trying to wrap my head around this issue and code ...

> In the last one, I put the code 'DATA_TransferCompleteRx();' in the comment line of the DMA interrupt and tried to restart the debugger. 

void DATA_TransferCompleteRx(void) { ... DATA_Send(gTxBuffer[i]); ... }

If I got that right, you trigger interrupt-driven transfers from within an interrupt handler.
Which doesn't strike me as a good idea.

Have you tried to observe the realtime SPI bus signals involved with a scope / logic analyser ?
If so, seems the code to "freeze" at about the same location ?

> My target hardware is NXP MKM34Z256VLL7. I tried ST as master and also ST as slave but I got the same problem in receive mode in both.

Are both MCUs on the same board & power supply ?
In other words, have you ruled out an electrical issue ?

redsire
Associate II

Hello,

 

I tried another debugger (J-Link) and it worked, then I tried connecting with ST-Link V2 again and it worked too.

Thanks to everyone who tried to help.

Some (or most) SWD/JTAG debug pods have the capability to supply power to the debuggee.
Check this option is not enabled, unless you really want to use it.