cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H523CE RTC wakeup

thansen
Associate II

I want to use the on-board RTC while all power (except VBAT which will be connected to a battery) is turned off to retain the clock.

Is it possible to power the on-board RTC from VBAT and turn off ALL other supplies?

What will happen after the other supplies are turned on again together with a POR?

Can one of the VBAT GPIOs be used to signal an RTC event with only VBAT powered (want to use this to wakeup)?

1 ACCEPTED SOLUTION

Accepted Solutions
PGump.1
Senior III

Hi,

Yes you can. Use the RTC_OUT pin to control VCC.

Kind regards
Pedro

 

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.

View solution in original post

5 REPLIES 5

> Is it possible to power the on-board RTC from VBAT and turn off ALL other supplies?

Yes. That's the purpose of VBAT.

> What will happen after the other supplies are turned on again together with a POR?

What would you expect to "happen"?

> Can one of the VBAT GPIOs be used to signal an RTC event with only VBAT powered (want to use this to wakeup)?

I don't know what do you mean by "RTC event", but reading the Power, RTC and TAMP chapters in RM will answer your question.

JW

 

PGump.1
Senior III

Hi,

Yes you can. Use the RTC_OUT pin to control VCC.

Kind regards
Pedro

 

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.

I want to wake up at a specific time.

Thank you Pedro I think that answers my question.

Thanks Pedro for the precise answer.