2023-12-01 08:45 AM
hi:
I have two NUCLEO-H563ZI EVB boards and tried to implement I3C controller and target feature.
When ENTDAA was issued, I obtained the target 48-bit provisioned ID "0x020813810100" from waveform, I saw the description from I3C register I3C_EPIDR ,it said" Bits[31:16] of the provisioned ID can be 0" but I got the actual value is "0x1381",so where is this value stored?
In addition, it seems that the target can issue a 48 bit provided ID without software operation , is this sending process entirely completed by MCU hardware?
2024-11-20 01:16 PM
So can I connect one ILPS28QSW and assign it to a dynamic address, then connect the second one with another dynamic address, so on so forth, finaly connect let's say 10 of them and get them working? THX!