cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 HAL_FLASHEx_OBGetConfig gives incorrect EDATASize

PieterG
Associate III

When I configure 8 EDATA sectors with

FLASH_OBInitStruct.OptionType = OPTIONBYTE_EDATA;
FLASH_OBInitStruct.Banks = FLASH_BANK_1;
FLASH_OBInitStruct.EDATASize = 8;
HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct);

 

and then I read the result:

 

FLASH_OBInitStruct.Banks = FLASH_BANK_1;
HAL_FLASHEx_OBGetConfig(&FLASH_OBInitStruct);

The FLASH_OBInitStruct.EDATASize member has the value 3.

 

This is caused by two issues:

In CMSIS/Device/stm32h563xx.h (and 562xx, 573xx and 503xx as well)

#define FLASH_EDATAR_EDATA_STRT_Msk (0x3UL << FLASH_EDATAR_EDATA_STRT_Pos) /*!< 0x00000003 */

while according to the datasheets this field is 3 bits wide:

PieterG_0-1701332072748.png

I've changed the mask to 0x7.

Now when I read EDATASize, I get the value of 7 (instead of 8).

This is because FLASH_OB_EDATAConfig uses EDATASize - 1, but FLASH_OB_EDATAConfig fails to add 1 to the result.

I've modified FLASH_OB_GetEDATA to add 1 to EDATASize, and also made a check on FLASH_EDATAR_EDATA_EN to avoid that zero FLASH_EDATAR_EDATA_STRT would result in EDATASize being 1:

/* Get configuration of secure area */
if (regvalue & FLASH_EDATAR_EDATA_EN)
{
  *EDATASize = (regvalue & FLASH_EDATAR_EDATA_STRT) + 1;
}

instead of what is currently used:

/* Get configuration of secure area */
*EDATASize = (regvalue & FLASH_EDATAR_EDATA_STRT);

 

Do you think these changes are correct, and if so, could you please apply them to STM32CubeH5?

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hello @PieterG 


Thank you to bring this issue to our attention. An internal ticket 167670 is submitted to update CubeH5.  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


View solution in original post

1 REPLY 1
FBL
ST Employee

Hello @PieterG 


Thank you to bring this issue to our attention. An internal ticket 167670 is submitted to update CubeH5.  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.