cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G491 datasheet echo!

Andrew Neil
Super User

The sentence "Exposure to maximum rating conditions for extended periods may affect device reliability" is repeated:

AndrewNeil_0-1727438152006.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
2 REPLIES 2
STTwo-32
ST Employee

Hello @Andrew Neil 

Thank you so much for reporting this typo. I've report it to the concerned team for correction on the coming releases (under internal ticket number 192316).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Karl Yamashita
Principal

ST is making sure you didn't miss reading it the first time and it sticks to your memory

KarlYamashita_0-1727454041725.jpeg

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source