cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G491 MCU Power Delivery Specification

MB.13
Associate II

Hi STM Team, 

 

We are planning to use STM32G491 MCU in our application. As per datasheet, it is mentioned that STM32G491 MCU will support USB PD 3.0.

 

We have come across the below STM document where it is mentioned that "STM32 UCPD MCUs are compliant with the latest USB PD r3.1 specifications" and EPR support is there.

 

Could you please confirm, whether STM32G491 MCU supports USB PD 3.1 and Extended Power Range Support(upto 240W).

 

Warm Regards,

Mythili B

 

5 REPLIES 5
FBL
ST Employee

Hi @MB.13 

Yes, the STM32G491 MCU supports the USB Power Delivery (USB PD) 3.1 specification, including features like Extended Power Range (EPR) for up to 240W. However, this support is contingent on using an updated software stack, such as the X-CUBE-TCPP middleware, which implements the USB PD 3.1 standard.

Support for USB PD 3.1, including features like Extended Power Range (EPR) (up to 240W), is primarily determined by the software stack rather than the UCPD hardware itself. The USB PD 3.1 standard introduces new messaging and behaviors, such as EPR mode, which are implemented in the software stack like X-CUBE-TCPP.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
MB.13
Associate II

Hi,

Thanks for your reply.

Can you also please suggest any port protection ICs like TCPP01-M12 for EPR(240W) sink applications.

We have seen in the datasheet of TCPP01-M12, where maximum voltage is 24V. But for our EPR application, max Voltage atleast protection IC should support 48V.

 

Warm Regards,

Mythili B 

Hi,

 

Any update on this?

 

Warm Regards,

Mythili B

Hi @MB.13 

Our expert @MROUV.1 can help you.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

Hi Mythili

STM32 embeds a solution compliant with USB-C PD r3.2 specifications, the last revision of the standard.

Indeed, thanks to its partitionning, solution follows lastest USB-PD release. Nevertheless, STM32 documentations are not updated at each USB PD release.

 

It’s keys a grant a maximum compliancy period of final product.

As exemple, the certification deadline for USB PD 3.1 v1.8 Silicon and End-Products has been extended to March 2026.

 

USB-PD has introduced the 48V possibility with PD 3.1 but 48V is not required to be compliant with 3.1 or higher.

 

Current solutions are up to 20V (100W) with TCPP series compliant with USB-C PD r3.2 specifications.

About 48V (240W), STMicroelectronics has not included solution to interface this voltage.

 

Best regards,

Mathieu