2024-11-28 2:25 AM
#include "Main.h"
#define MAX_Intensity 1600
static volatile uint16_t Intensity = 10;
void Timer4_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_BaseStructure;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
TIM_BaseStructure.TIM_Prescaler = 1 - 1;
TIM_BaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_BaseStructure.TIM_Period = MAX_Intensity - 1;
TIM_BaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseInit(TIM4, &TIM_BaseStructure);
TIM_Cmd(TIM4, ENABLE);
}
void PWM_Configuration()
{
TIM_OCInitTypeDef TIM_OCStructure;
TIM_OCStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCStructure.TIM_Pulse = 0;
TIM_OC1Init(TIM4, &TIM_OCStructure);
TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OC2Init(TIM4, &TIM_OCStructure);
TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OC3Init(TIM4, &TIM_OCStructure);
TIM_OC3PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OC4Init(TIM4, &TIM_OCStructure);
TIM_OC4PreloadConfig(TIM4, TIM_OCPreload_Enable);
}
void GPIO_PWM_Configuration()
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource13, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_TIM4);
GPIO_InitStructure.GPIO_Pin = ALL_LEDS;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
void TIM2_Configuration(u32 Intervalms)
{
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_TimeBaseStructure.TIM_Prescaler = 16000-1;
TIM_TimeBaseStructure.TIM_Period = Intervalms-1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);
TIM_Cmd(TIM2, ENABLE);
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);
NVIC_InitTypeDef NVIC_InitStructure;
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
int main(void)
{
GPIO_PWM_Configuration();
Timer4_Configuration();
PWM_Configuration();
TIM2_Configuration(500);
while(1)
{
}
}
void TIM2_IRQHandler()
{
if(TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
{
if(Intensity > MAX_Intensity)
{
Intensity = 10;
}
TIM4->CCR1 = Intensity;
TIM4->CCR2 = Intensity;
TIM4->CCR3 = Intensity;
TIM4->CCR4 = Intensity;
Intensity = Intensity * 2;
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
}
}
The code above is the example I am referring to. However, the Timer2 interrupt does not occur in this code. However, if you change the Timer2Configuration function call to before the PWM_Configuration function call, the interrupt operates normally. I can't find the cause of this behavior, so I'm asking a question.
i'm conducting practice using STM32F407G-DISC1.
Solved! Go to Solution.
2024-11-28 4:06 AM
int main(void)
{
GPIO_PWM_Configuration();
TIM2_Configuration(500);
Timer4_Configuration();
PWM_Configuration();
while(1)
{
}
}Try like this.
2024-11-28 3:08 AM
Hello @treeset, welcome to ST community,
I think that the part in the TIM2 configuration that makes it work is the NVIC configuration, it's mandatory to configure the NVIC before enabling interrupts
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-28 4:06 AM
int main(void)
{
GPIO_PWM_Configuration();
TIM2_Configuration(500);
Timer4_Configuration();
PWM_Configuration();
while(1)
{
}
}Try like this.
2024-11-28 5:32 PM
If you make this modification, PWM will operate normally. However, I think it is strange that it works normally even though I simply changed the calling order. Do you know what the cause is?
2024-12-03 5:50 AM
The issue occurs because the NVIC_PriorityGroupConfig() function, which sets the interrupt priority grouping, must be called before any interrupt configurations; if you call PWM_Configuration() before TIM2_Configuration(), it's possible that PWM_Configuration() or functions it invokes alter the NVIC settings, overwriting the priority settings for TIM2 and preventing its interrupt from occurring; by moving the NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); call to the very beginning of main()—before any other configurations—you ensure that the priority grouping is set correctly before any interrupts are configured, which resolves the issue.
2024-12-04 1:30 AM
Thanks for your help bruh