2022-11-12 5:36 AM
how disable boot 0 pin8 i used this pin for input make problem to boot from flash how can disable any condition mcu boot from flash not check this pin when reset
Solved! Go to Solution.
2022-11-13 6:04 AM
you can set the related option bytes to avoid the boot pin impact.
you can check the Boot configuration part of the reference manual.
nBOOT0 FLASH_OPTR[27] set to 1, and nSWBOOT0 FLASH_OPTR[26] set to 0 will make the chip boot from main flash and regard less of the boot pin.
2022-11-12 6:02 AM
You've post this 6 times, please don't do that. Edit posts if you need to add or change details.
Check if there are Option Byte settings to fix nBOOT, or similar
2022-11-12 7:45 PM
I SEND ONE TIME 6 TIME GOT MASAGE TRAY AGAIN
I USED PB8 FOR INPUT WHEN RESET IF THIS PIN HIGH NOT BOOT FROM INTERNAL FLASH I TRY TO FINED WAY HOW CANCEL THIS PIN NO ANY EFECT ON BOOT ADDRESS ALL CONDITION BOOT FROM INTERNAL FLASH MEMORY
2022-11-13 6:04 AM
you can set the related option bytes to avoid the boot pin impact.
you can check the Boot configuration part of the reference manual.
nBOOT0 FLASH_OPTR[27] set to 1, and nSWBOOT0 FLASH_OPTR[26] set to 0 will make the chip boot from main flash and regard less of the boot pin.
2022-11-13 11:16 PM
is possible example software give me how to do it becuse after reset cpu go to one address start
nSWBOOT0 FLASH_OPTR[26] and nBOOT0 FLASH_OPTR[27] this register or flash address must write ?
2022-11-13 11:21 PM
you can use the cubeprogrammer to do the option byte configuration
2022-11-24 10:58 PM
thanks fixed my problems