cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4 - Run after programming

Atzosskin
Associate

Hello I hope you can help.

We have developed a production programming solution for the range of STM32G474 devices which uses our own hardware controller interface.

Is it possible to replicate the "run after programming" --go command externally?

(eg, without using the STM32CubeProgrammer CLI.exe)

As currently the boards do not boot after configuration.

Kind regards

Atz.

 

1 REPLY 1
Uwe Bonnes
Principal III

Describe your setup better. Does the board run a bootloader or do you programm via SWD/Jtag. In the first case, your own bootloader needs ti implement som "go" command. With SWD/JTAG a reset, even sent via SWD/JTAG wi help.