2025-01-20 06:24 AM
Hello and thank you for taking the time to read and answer my question.
What I want to do:
I have SYSCLK configured at a frequency of 16 MHz (using HSI), and a PLL block clock with a frequency of 18 MHz.
I want to sample the PLL clock on the rising edge of the SYSCLK. (the application in which I want to use this is not really of interest in this post).
What is the most efficient way to do this?
Use a timer channel in input capture mode for the reference clock and read the value of the other channel where I connect the 18 MHz clock, whenever I have a rising edge?
Interrupts? (It seems like 16.000.000 interrupts a second might saturate the CPU)
Any other good way?
2025-01-20 06:28 AM
Im not sure i fully grasp yopur needs, but what about DMA+ADC, using timer base without interruption? disabling DMA interruption aswell?, just thinkign outloud here.
The ADCs are supposed to be able to manage up to 64Mhz.
Did you already tried something?
2025-01-20 06:53 AM
What is "PLL block"? Some external circuitry?
JW
2025-01-20 04:53 PM
@Javier1 wrote:...
The ADCs are supposed to be able to manage up to 64Mhz.
..
The adc can be run faster but the sampling time still has its limits.
2025-01-21 12:39 AM
No, when I say PLL block I'm referring to the three clocks (PLLRCLK, PLLQCLK and PLLPCLK) which can be generated internally, the phased locked loop clocks.
2025-01-21 12:43 AM - edited 2025-01-21 12:55 AM
@Carl_G wrote:
@Javier1 wrote:...
The ADCs are supposed to be able to manage up to 64Mhz.
..The adc can be run faster but the sampling time still has its limits.
Interesting, giving the fact I only need to know if the current clock pulse value is either a logic 1 or a 0, I don't mind truncating the resolution at all, 6 bits is more than enough, but it still seems I'm using a bit much.
Can't GPIO support 16MHz access to the input of the pin and just configure a timer with the frequency of the reference 16 MHz clock to generate a gpio read on each rising edge event?
2025-01-21 01:45 AM
I cannot be of much help here, never done that fast adquisition, what youre trying to do is very interesting post your findings here please.
(How about DMA accessing GPIO state register?)
2025-01-21 05:39 AM - edited 2025-01-21 05:45 AM
If all you need is a 1 or a 0 then what you want is called Input Capture. I reread your post. I think you are maybe using some terms wrong or misunderstanding something.
If you want to measure the signal on a certain GPIO using an input capture timer that is running on the PLL that's totally doable. However, according to the Nyquist theory you want your sampling clock to be at least twice as fast as your sampled clock. So if your input signal is 18MHz then you should run your sampling clock of your timer at least 36MHz. Are you trying to measure frequency, or duty cycle or pulse width? Techniques will depend on which.
2025-01-21 08:40 AM
My understanding of the initial post is, that the intention is to clock timer using 16MHz sysclk while somehow characterize a 18MHz signal, whatever is it's source, and in whatever way is it routed to the timer (which remains to be a question - connecting TIMx_CHx to MCO externally, perhaps?)
While this most probably won't result in anything reasonable, the question is: why? The final target may or may not be within reach, but if yes, most probably not in the proposed way.
JW
2025-01-21 09:43 AM
This is my setup:
HSI16 to MCO and connected externally to a GPIO pin.
PLLQCLK of 18 MHz to MCO2 and connected externally to TIM16_CH1.
Configured TIM16 in input capture mode, generate an interrupt on capture event and poll the GPIOx IDR register for its value.
Why now:
I made two other posts in my attempt to reproduce a small random number generator. Again, it's just an attempt.
What I'm trying to base my attempt on is the intrinsic time jitter the PLL clock has (which I measured as well using an oscilloscope). Sampling the PLL clock with a specific frequency I choose (16MHz) is another attempt at reproducing the research I found here: True Random Number Generator Embedded in Reconfigurable Hardware