2023-01-06 7:01 AM
Greetings!
I was trying to make a host device on STM32G0 to access system Bootloader of another STM32G0B1CBT6 to update Firmware over CANFd. Reference was taken from "AN5405"
I configured the host device as mentioned in Application note and tried to the "GET Command" on CAN ID from 0x00 to 0x7ff, but i didn't received any response from system bootloder. Configuration of host is as below:
Clock Frequency: 20Mhz
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 16;
hfdcan1.Init.NominalTimeSeg1 = 63;
hfdcan1.Init.NominalTimeSeg2 = 16;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 4;
hfdcan1.Init.DataTimeSeg1 = 15;
hfdcan1.Init.DataTimeSeg2 = 4;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
FilterConfig.IdType = FDCAN_STANDARD_ID;
FilterConfig.FilterIndex = 0;
FilterConfig.FilterType = FDCAN_FILTER_RANGE;
FilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
FilterConfig.FilterID1 = 0;
FilterConfig.FilterID2 = 0x7ff;
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &FilterConfig) != HAL_OK)
{
CAN_FD_ErrorCode = CAN_FD_ConfigFiltterError;
CAN_FaultStatus = true;
globalErrorStatus = true;
Error_Handler();
}
/* Configure global filter:
Filter all remote frames with STD and EXT ID
Reject non matching frames with STD ID and EXT ID */
if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_FILTER_TO_RXFIFO0, FDCAN_FILTER_TO_RXFIFO0, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
{
CAN_FD_ErrorCode = CAN_FD_GlobalFillterError;
CAN_FaultStatus = true;
globalErrorStatus = true;
Error_Handler();
}
/* Activate Rx FIFO 0 new message notification */
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
{
CAN_FD_ErrorCode = CAN_FD_RxFifoActivationError;
CAN_FaultStatus = true;
globalErrorStatus = true;
Error_Handler();
}
/* Prepare Tx message Header */
txHeader.Identifier = 0x1;
txHeader.IdType = FDCAN_STANDARD_ID;
txHeader.TxFrameType = FDCAN_DATA_FRAME;
txHeader.DataLength = FDCAN_DLC_BYTES_64;
txHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
txHeader.BitRateSwitch = FDCAN_BRS_ON;
txHeader.FDFormat = FDCAN_FD_CAN;
txHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
txHeader.MessageMarker = 0;
/* Configure and enable Tx Delay Compensation, required for BRS mode.
TdcOffset default recommended value: DataTimeSeg1 * DataPrescaler
TdcFilter default recommended value: 0 */
if (HAL_FDCAN_ConfigTxDelayCompensation(&hfdcan1, 5, 0) != HAL_OK)
{
CAN_FD_ErrorCode = CAN_FD_ConfigTxDelayError;
CAN_FaultStatus = true;
globalErrorStatus = true;
Error_Handler();
}
if (HAL_FDCAN_EnableTxDelayCompensation(&hfdcan1) != HAL_OK)
{
CAN_FD_ErrorCode = CAN_FD_EnableTxDelayError;
CAN_FaultStatus = true;
globalErrorStatus = true;
Error_Handler();
}
/* Start the FDCAN module */
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
CAN_FD_ErrorCode = CAN_FD_StartError;
CAN_FaultStatus = true;
globalErrorStatus = true;
Error_Handler();
}
During transmission of CAN packet i used to change Tx Identifier from range of 0x00 to 0x7ff.
Also Data Length was tried both 0 and 1 as mentioned in Application note.
Any help would be appriciated.
Thanks,
Tirthraj Solanki
2023-01-06 9:21 AM
Primary you check if client is in bootloader mode.
Secondary your connection need on client be as AN2606 only pin PD0 PD1
2023-01-06 9:36 PM
Hi,
Thank you for your response.
So, yes client is in bootloader mode, verified by using UART protocol.
Also pin used for CANFd are PD0 and PD1.
2023-01-07 2:50 AM
Ok then bootloader maybe detect some other interface or you have mistake , protocol speed 0.5M?
2024-12-05 10:47 PM - last edited on 2024-12-06 12:00 AM by mƎALLEm
1. FDCAN clock error in SystemClock_Cnfig() function in the original project,
You can use the function:
canClockFreqkHz = LL_RCC_GetFDCANClockFreq(LL_RCC_FDCAN_CLKSOURCE) / 1000u;
Get the value of canClockFreqkHz as 30MHz
2. Modify the SystemClock_Cnfig() function to use an external crystal at 8MHz:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
//HSE: 8MHz----Config: SYS CLK:60MHz; FDCAN CLK:20MHz----USB: HSI48[48MHz]
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_HSI48;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV2;
RCC_OscInitStruct.PLL.PLLN = 30;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV6;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
3. Modify the OPENBL_SDCAN-INnit() function in the fdcan_interface. c file:
static void OPENBL_FDCAN_Init(void)
{
/* Bit time configuration:
Bit time parameter | Nominal | Data
---------------------------|--------------|----------------
fdcan_ker_ck | 20 MHz | 20 MHz
Time_quantum (tq) | 50 ns | 50 ns
Synchronization_segment | 1 tq | 1 tq
Propagation_segment | 23 tq | 1 tq
Phase_segment_1 | 8 tq | 4 tq
Phase_segment_2 | 8 tq | 4 tq
Synchronization_Jump_width | 8 tq | 4 tq
Bit_length | 40 tq = 2 us | 10 tq = 0.5 us
Bit_rate | 0.5 MBit/s | 2 MBit/s
*/
hfdcan.Instance = FDCANx;
hfdcan.Init.FrameFormat = FDCAN_FRAME_FD_BRS;
hfdcan.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan.Init.AutoRetransmission = ENABLE;
hfdcan.Init.TransmitPause = DISABLE;
hfdcan.Init.ProtocolException = ENABLE;
#if 0 //Error!
hfdcan.Init.NominalPrescaler = 0x1;
hfdcan.Init.NominalSyncJumpWidth = 0x10;
hfdcan.Init.NominalTimeSeg1 = 0x3F;
hfdcan.Init.NominalTimeSeg2 = 0x10;
hfdcan.Init.DataPrescaler = 0x1;
hfdcan.Init.DataSyncJumpWidth = 0x4;
hfdcan.Init.DataTimeSeg1 = 0xF;
hfdcan.Init.DataTimeSeg2 = 0x4;
#else //Correct
hfdcan.Init.NominalPrescaler = 0x01;
hfdcan.Init.NominalSyncJumpWidth = 0x8;
hfdcan.Init.NominalTimeSeg1 = 0x1F;
hfdcan.Init.NominalTimeSeg2 = 0x8;
hfdcan.Init.DataPrescaler = 0x01;
hfdcan.Init.DataSyncJumpWidth = 0x4;
hfdcan.Init.DataTimeSeg1 = 0x05;
hfdcan.Init.DataTimeSeg2 = 0x04;
#endif
hfdcan.Init.StdFiltersNbr = 1;
hfdcan.Init.ExtFiltersNbr = 0;
hfdcan.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan) != HAL_OK)
{
while (1);
}
/* Configure Rx filter */
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x111;
sFilterConfig.FilterID2 = 0x7FF;
HAL_FDCAN_ConfigFilter(&hfdcan, &sFilterConfig);
/* Prepare Tx Header */
TxHeader.Identifier = 0x111;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_64;
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_ON;
TxHeader.FDFormat = FDCAN_FD_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
/* Start the FDCAN module */
HAL_FDCAN_Start(&hfdcan);
}
4. Set a breakpoint at the detected=1 position in the
OPENBL_SDCAN-ProtocolDetection() function,
and you will get detected=1,
5. Test OK