2022-06-17 11:02 PM
I wanted to know which channel is converted latest. I configured as below
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_SEQ_FIXED;
hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV; //
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.LowPowerAutoPowerOff = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE; //
hadc1.Init.NbrOfConversion = 4;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T6_TRGO; //
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; //
hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_1CYCLE_5;
hadc1.Init.OversamplingMode = DISABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_4;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
in the call back function
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
/* Retrieve ADC conversion data */
uhADCxConvertedData = HAL_ADC_GetValue(hadc);
/* Computation of ADC conversions raw data to physical values */
/* using helper macro. */
//uhADCxConvertedData_Voltage_mVolt = __ADC_CALC_DATA_VOLTAGE(VDDA_APPLI, uhADCxConvertedData);
/* Update status variable of ADC unitary conversion */
ubAdcGrpRegularUnitaryConvStatus = 1;
ADCcount++;
if(ADCcount > 1000)
{
ADCcount = 0;
HAL_GPIO_TogglePin (LED3_GPIO_Port, LED3_Pin);
}
}
I wanted know which channel was last converted.
2022-06-18 8:49 AM
Since you haven't changed the rank for each channel, you will probably get 4 conversions of Channel 4.
Edit: Unless you really want to reconfigure the ADC after each channel, it is best to use DMA for more than one channel. There is probably a DMA example in the G0 library examples.
Cheers, Hal