cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G070RB as Slave and ESP32 S3 C1 devkit as Master, I2C Bootloader

RamyaD
Associate II

Hi,

i am using STM32G070RB as Slave and ESP32 S3 C1 devkit as Master, Need to implement I2C Bootloader for stm32 from esp32. Can anyone help me with this.

 

Thanks in advance

1 REPLY 1
Peter BENSCH
ST Employee
If you want to program via I2C, you can use the internal bootloader and the AN4221 as a basis for your own development.
 
Hope that helps?
 
Regards /Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.