2021-11-30 3:17 PM
I have a strange issue. I use printf function in a uart port for print some variables that I use in my code. This works perfectly in cortex m4, but now in cortex m0, the variable printed show me 0, in the next code:
uint8_t flash_ext_init(void){
uint8_t wr_word[4];
uint8_t rd_word[4];
printf("Loading flash memory BY25Q32...\n");
// w25q_FirstFallingCS();
memset(wr_word, 0, 4);
memset(rd_word, 0, 4);
wr_word[0] = W25Q_CMD_JEDEC_ID;
_flash_ext_spi_write_read_data(rd_word, wr_word, 4);
printf("Flash_stat: %02xh, %02xh, %02xh, %02xh\n", rd_word[0], rd_word[1], rd_word[2], rd_word[3]);
printf("BY25Q32 flash loaded...\n");
// printf("Flash_stat_reg1: %02xh, flash_stat_reg2: %02xh, flash_stat_reg3: %02xh...\n", w25qxx.StatusRegister1, w25qxx.StatusRegister2, w25qxx.StatusRegister3);
return 1;
}I am using -O2 optimization, and when I make a debugging process in stm32cube ide i can see that variables has the correct value, however when the variables are printed, this print a 0 value. I have test disabling "strict aliasing" in optimization settings. And the issue is solved. However, I think is better enable this optimization flag.
2021-11-30 4:10 PM
Looks like I am accesing too fast to the variable, when I add a hal_delay of 1 ms after _flash_ext_spi_writ... and before printf, the variable is printed correctly. I am following this procedure to wait for complete dma transfer:
static void _flash_ext_spi_start_wait_stop_dma_transaction(void){
LL_SPI_Enable(FLASH_EXT_SPI_HANDLER);
while(FLASH_EXT_DMA_WAIT_FOR_TX); // while(LL_DMA_IsActiveFlag_TC4(FLASH_EXT_DMA_HANDLER) == 0);
while(LL_SPI_GetTxFIFOLevel(FLASH_EXT_SPI_HANDLER) != LL_SPI_TX_FIFO_EMPTY);
while(LL_SPI_IsActiveFlag_BSY(FLASH_EXT_SPI_HANDLER) != 0);
while(FLASH_EXT_DMA_WAIT_FOR_RX); // while(LL_DMA_IsActiveFlag_TC5(FLASH_EXT_DMA_HANDLER) == 0);
LL_SPI_Disable(FLASH_EXT_SPI_HANDLER);
while(LL_SPI_GetRxFIFOLevel(FLASH_EXT_SPI_HANDLER) != LL_SPI_RX_FIFO_EMPTY);
}then i disable the dma:
static void _flash_ext_spi_disable_dma(void){
LL_DMA_DisableChannel(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_RX);
LL_DMA_DisableChannel(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_TX);
LL_SPI_DisableDMAReq_RX(FLASH_EXT_SPI_HANDLER);
LL_SPI_DisableDMAReq_TX(FLASH_EXT_SPI_HANDLER);
}
2021-11-30 4:21 PM
Optimization 1 also solve the issue, I will use -O1 as workaround. If someone has deeply knowledge in compiler flags, I will be thankful.
2021-11-30 7:17 PM
What's in _flash_ext_spi_write_read_data? Seems like you're using DMA. Probably rd_word needs to be marked volatile.
2021-11-30 8:48 PM
static void _flash_ext_spi_config_dma(uint32_t *mem_read_address, uint32_t *mem_write_address, uint32_t length){
LL_SPI_SetRxFIFOThreshold(FLASH_EXT_SPI_HANDLER, LL_SPI_RX_FIFO_TH_QUARTER);
LL_DMA_SetMode(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_RX, LL_DMA_MODE_NORMAL);
LL_DMA_SetDataTransferDirection(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_RX, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_DMA_SetPeriphAddress(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_RX, LL_SPI_DMA_GetRegAddr(FLASH_EXT_SPI_HANDLER));
LL_DMA_SetMemoryAddress(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_RX, (uint32_t)mem_read_address);
LL_DMA_SetDataLength(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_RX, length);
LL_DMA_EnableChannel(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_RX);
LL_SPI_EnableDMAReq_RX(FLASH_EXT_SPI_HANDLER);
LL_DMA_SetMode(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_TX, LL_DMA_MODE_NORMAL);
LL_DMA_SetDataTransferDirection(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_TX, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetPeriphAddress(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_TX, LL_SPI_DMA_GetRegAddr(FLASH_EXT_SPI_HANDLER));
LL_DMA_SetMemoryAddress(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_TX, (uint32_t)mem_write_address);
LL_DMA_SetDataLength(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_TX, length);
LL_DMA_EnableChannel(FLASH_EXT_DMA_HANDLER, FLASH_EXT_DMA_CHANNEL_TX);
LL_SPI_EnableDMAReq_TX(FLASH_EXT_SPI_HANDLER);
}
2021-11-30 8:48 PM
data is not handled in isr, it is filled by dma peripheral.
2021-11-30 8:58 PM
2021-12-01 7:37 AM
Could be a problem of too small stack or heap size. The Newlib's printf functions require huge amounts of both...
2021-12-01 10:33 PM
0x400 and 0x800 of size
2021-12-02 6:23 AM
One option is that you're not waiting for the DMA transfer to complete. But that's just a guess as you still haven't shown _flash_ext_spi_write_read_data.