Hello. Using NRST as an output. Initial state 1. After loading, I switch to 0 and the MCU is rebooted :(. I used options PA0, PA1, PA2. If I use PF2, then the output is constant 1. MCU stm32g031j6m6. On the STM32G0316-DISCO board, the same MPU works ...