2024-07-24 4:14 PM
Hi,
I'm trying to set my setup my SPI1 as slave full duplex on my STM32G030K8 and i reach the HAL_SPI_TxRxCpltCallback when receiving message, but I always read value 0 in my rxbuffer when my master is spamming 16 @ 1MHz at a 1 sec intervall. Also, my slave should be answering 196 base on the value place in the txbuff, but nothing seem to get out;
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef * hspi)
{
__disable_irq();
switch(spi_s.state)
{
case REG:
spi_s.reg = spi_s.rx_buff[1];
if(spi_s.rx_buff[0] & WRITE_MASK)
{
spi_s.state = VALUE;
}
else
{
manage_reg_read(spi_s.reg);
}
break;
case VALUE:
manage_reg_write(spi_s.reg);
break;
}
if(HAL_SPI_TransmitReceive_IT(&hspi1, (uint8_t*)spi_s.tx_buff, (uint8_t*)spi_s.rx_buff, SPI_BUFF_SIZE))
{
Error_Handler();
}
__enable_irq();
}
void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin)
{
__disable_irq();
spi_s.reg = 0;
spi_s.state = REG;
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
hspi1.Instance->CR1 |= (1<<SPI_CR1_SSI_Pos);
//HAL_SPI_TransmitReceive_IT(&hspi1, (uint8_t*)spi_s.tx_buff, (uint8_t*)spi_s.rx_buff, sizeof(uint16_t));
__enable_irq();
}
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
__disable_irq();
switch(GPIO_Pin)
{
case CS_Pin:
HAL_SPIEx_FlushRxFifo(&hspi1);
hspi1.Instance->CR1 &=(~SPI_CR1_SSI_Msk);
break;
case PIR_Pin:
case Button_Pin:
init_clock();
init_GPIO();
while( HAL_GPIO_ReadPin(Button_GPIO_Port, Button_Pin));
break;
}
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
__enable_irq();
}
void init_SPI()
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
for(uint8_t i = 0; i < SPI_BUFF_SIZE;i++)
{
spi_s.rx_buff[i] = 0;
spi_s.tx_buff[i] = 0;
}
spi_s.reg = 0;
spi_s.state = REG;
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIOA->MODER |= (0x02<<GPIO_MODER_MODE2_Pos)|((0x02<<GPIO_MODER_MODE5_Pos))|((0x02<<GPIO_MODER_MODE6_Pos));
GPIOA->OSPEEDR |= (11<<GPIO_OSPEEDR_OSPEED2_Pos)|(11<<GPIO_OSPEEDR_OSPEED5_Pos)|(11<<GPIO_OSPEEDR_OSPEED6_Pos);
GPIOA->AFR[0] &= (~GPIO_AFRL_AFSEL2_Msk)&(~GPIO_AFRL_AFSEL5_Msk)&(~GPIO_AFRL_AFSEL6_Msk);
GPIO_InitStruct.Alternate = GPIO_AF0_SPI1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pin = SCK_Pin;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(SCK_GPIO_Port, &GPIO_InitStruct);
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pin = INT_Pin;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(INT_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : CS_Pin */
GPIO_InitStruct.Pin = CS_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(CS_GPIO_Port, &GPIO_InitStruct);
__HAL_RCC_SPI1_CLK_ENABLE();
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
// cs int
HAL_NVIC_SetPriority(EXTI2_3_IRQn, IRQ_SPI_PRIORITY, 0);
HAL_NVIC_EnableIRQ(EXTI2_3_IRQn);
HAL_NVIC_SetPriority(SPI1_IRQn, IRQ_SPI_PRIORITY, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
if(HAL_SPI_TransmitReceive_IT(&hspi1, (uint8_t*)spi_s.tx_buff, (uint8_t*)spi_s.rx_buff, SPI_BUFF_SIZE))
{
Error_Handler();
}
}
Blue: SCK Yellow: Mosi
Yellow: MISO Blue:SCK
Thank you!
Solved! Go to Solution.
2024-08-15 7:59 AM
Sorry for the delay it seem like it was a hardware problem, i change the chip and now it work
2024-07-24 11:54 PM
Incorrect MISO/MOSI setup in GPIO?
Read out and check/post content of relevant GPIO registers.
JW
2024-08-15 7:59 AM
Sorry for the delay it seem like it was a hardware problem, i change the chip and now it work