cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32G030K6T] / low power sleep / power consumption / 116uA instead of 13uA

RRIDDICC
Associate II

Hi!

When i run this code in SRAM via the UART bootloader "go command":

 

asm("cpsid i\n"); // turn off prefetch and set FLASH.latency to 0 cFicen(); cFprften(); uFlatency(0); while (gFlatency()!=0); // config GPIO (seems to have no effect on power consumption) ((u32*)GPIO[A])[MODER]=-1U; ((u32*)GPIO[A])[OSPEEDR]=0; ((u32*)GPIO[A])[PUPDR]=0; ((u32*)GPIO[C])[MODER]=-1U; ((u32*)GPIO[D])[MODER]=-1U; ((u32*)RCC)[IOPENR]=0; // switch sysclk to LSI and turn off HSI (initial letter:s=set,c=clr,g=get,u=update) sClsion(); while (!gClsirdy()); uCsw(LSI); while (gCsws()!=LSI); cChsion(); // go to low power run mode sPlpr(); // go to low power sleep mode while (!gPreglpf()); cSCRsleepdeep(); asm("wfi\n");

 

I get a current of 136uA, where the external parts (PCA9306, SP0504, 2 LDOs, NCP431 voltage clamp) use 20uA...

Even in "run mode"/range2/SRAM/8MHz it used 728uA, instead of the typical 600uA+20uA.

Can someone here say, how i can save those 100uA?

Should I try another board without all those extra parts? Just the STM32G030K6T and a cap of course...?

Thx.

Bye.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Piranha ,

Thank you for your reply.

I found that PWR's clock needs to be enabled in RCC->APBENR1 (PWREN: bit#28). So i added a "sCpwren();"... and it works now: 23µA (with standby mode...)... ChatGPT mentioned that PWR registers need love a clock, too... :face_with_tears_of_joy: :rolling_on_the_floor_laughing:

postscriptum: Now I will try to take care of the compiler optimizations... CMSIS has really some advantages (but i would have to type (or use vim's CTRL+p) a lot...)... GCC seems to be a little bit funny (e. g. it adds a "cmp" after a "subs" in loops, to find out if "subs" resulted in "zero", although "subs" should already take care of that...)... :grinning_face:

Best Regards.

View solution in original post

7 REPLIES 7
Issamos
Lead II

Hello @RRIDDICC 

For sure, using a board with just the necessary elements will help reducing the energy consommation.

Best regards.

II

Piranha
Chief II

You didn't even tell what low-power mode are you trying to enter. Anyway, the related issues and proper code is explained there:

https://community.st.com/t5/stm32-mcus-embedded-software/how-to-enter-standby-or-shutdown-mode-on-stm32/m-p/145849

Your has many problems also - register accesses are not volatile, inline ASM is missing compiler barriers and nobody knows what other broken code is hidden in all of those strangely named functions. Not using CMSIS provided register definitions and macros doesn't make a sense and leads exactly to such a disaster.


@Piranha wrote:

You didn't even tell what low-power mode are you trying to enter.

Not using CMSIS provided register definitions and macros doesn't make a sense


  1. low power sleep (mentioned in DS12991 Rev 3 page 45 table 26, but clocked by LSI instead of LSE)
  2. hmm... where can i find those CMSIS definitions&macros for arm-none-eabi-gcc?
  3. would u like to see the disassembled elf file?
Piranha
Chief II

Ah, you actually already told it... Anyway, read my article because part of it is relevant for all low-power modes.

How can one find the MCU, datasheet, reference manual and this forum, but then not find the provided code?

https://www.st.com/en/embedded-software/stm32cubeg0.html

https://github.com/STMicroelectronics/STM32CubeG0/tree/master/Drivers/CMSIS/Device/ST/STM32G0xx/Include

https://github.com/ARM-software/CMSIS_5/tree/develop/CMSIS/Core/Include

Hello @Issamos ,

Tthank you for your reply.

I tried a board with the µC and 2 ceramic caps only and the result of the unchange code was the same.

Best regards.

Hello again,

Try this post. It may help you.

Best regards.

II

Hello @Piranha ,

Thank you for your reply.

I found that PWR's clock needs to be enabled in RCC->APBENR1 (PWREN: bit#28). So i added a "sCpwren();"... and it works now: 23µA (with standby mode...)... ChatGPT mentioned that PWR registers need love a clock, too... :face_with_tears_of_joy: :rolling_on_the_floor_laughing:

postscriptum: Now I will try to take care of the compiler optimizations... CMSIS has really some advantages (but i would have to type (or use vim's CTRL+p) a lot...)... GCC seems to be a little bit funny (e. g. it adds a "cmp" after a "subs" in loops, to find out if "subs" resulted in "zero", although "subs" should already take care of that...)... :grinning_face:

Best Regards.