STM32F767ZI USART abnormal Rx in interrupt mode
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-14 2:58 AM
I do my code with CUBEMX 5.6.0 with en.STM32Cube_FW_F7_V1.16.0 & Atollic 9.2.0.
My trouble :
when i send a data by USART3 (using putty or the terminal in Atollic) even if i set that i want to recive 1 byte the HAL_UART_RxCpltCallback is fired two time (like i set i want recive 2 byte), why it happen? What wrong i do?
I attach the file that i write/change using CUBEMX & Atollic => main.c & stm32f7xx_it.c, and a screenshot.
I try some solution (are commented inside the function) but i don't find one.
In the picture you can see:
1) If i send only one char, in the console i see the char that i send and an \r (i see it using debug ), and no error occured;
2) If i send 2 char, in the console i see the 2 char that i send, and no error occured;
3) If i send 3 char, in the console i see only 2 char, and no error occured;
I write HAL_UART_ErrorCallback in this way only for debug test.
- Labels:
-
STM32F7 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-15 2:15 AM
FIND SOLUTION:
s1) See the picture.
s2) In the Putty configuration terminal last time i have seeting Local line editing = Force on and i have the trouble, today i set Local line editing = Force off and and the behaviour of the transmission gone right; i suppose that if i set 1st config the press of ENTER is sent (isn't only a wait used by putty to transmit when i want) so i have the trouble.
s3) If i sent from putty a char that is in the extend ascii table, the behaviour is like that i sent two byte but it is not right subdivide in two byte??
NOW I HAVE SOME QUESTIONS:
q1) why the behaviour that i said in point "s3" is like this ?
q2) where in Atollic i can configure the right procotol like in Putty (i supposed that the trouble is generated like in point "s2" for Putty) ?
q3) the code that i have writed is the right way to operate ? or ther is a better way?
Thank you.