2017-02-27 8:11 AM
RM0410, rev.2 defines 0xF0FFAAFD as default value for FLASH_OPTCR. Table 3.7.8 has a value of 0xFFFFAAFD. This value does make more sense.
Please correct, if not yet already done.
Solved! Go to Solution.
2018-04-06 1:28 AM
Hello,
FLASH_OPTCR reset value u
pdated in Section 3.7.6: Flash option control register (FLASH_OPTCR) reset value at ‘0xFFFFAAFD’.Kind Regards,
Imen
2017-06-13 7:06 AM
Hi
Bonnes.Uwe
,Thank you for reported this error.
I highlighted this internally and it will be corrected in the coming release of the reference manual RM04
Regards
Imen
2018-04-06 1:28 AM
Hello,
FLASH_OPTCR reset value u
pdated in Section 3.7.6: Flash option control register (FLASH_OPTCR) reset value at ‘0xFFFFAAFD’.Kind Regards,
Imen
2018-04-06 4:04 AM
,
,
Is there a new revision of the H743 datasheet or reference manual?
does not tell so yet.