cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO

Michael Landis
Associate
Posted on April 20, 2017 at 12:22

Can someone please share the physical height of the STM32F746G Discovery board?  Length and width are in the manual, but height is very difficult to find.  Thanks

2 REPLIES 2
Posted on April 20, 2017 at 20:41

23mm

Imen.D
ST Employee
Posted on April 24, 2017 at 11:59

Hi

darksky

,

It's 23mm as mentioned by

Waclawek.Jan

.

Indeed,

the physical height with the screen is between22mmand 24mm(taking into account the thickness of the scotch double-sided in the screen) and t

he height without display screen is 15mm.

I would inform you that I have reported internally the missing information to take the necessary action and add the physical height for all manuals in coming release.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen