2019-07-04 5:40 AM
Hi Community,
I have a STM32F769I as a SPI slave.
I want to receive up to 6kByte data in 244 Byte packets (consequently up to 25 SPI packets á 244 Byte).
I am using the HAL_SPI_TxRxCpltCallback function. This function will be called after every 244 Byte packet; and stores the received data in a 6 kByte data buffer. After all data has been received a flag will be set to activate a print function in the main.
For now, the 6 kByte (dummy) data frames will be send every 2 seconds by the SPI master.
However, the STM32 sometimes misses SPI packets and consequently mess up the data.
As soon as I exceed an amount of data (4392 Byte = 18 packets á 244 bytes) the STM misses packets in a transaction and thus the data will only be printed after every second transaction.
Furthermore, memory access problems occure every now and then ending up in the HardFault_handler.
I think, I am facing some timing problems due to interrupts as well as memory access problems.
Any suggestions?
Solved! Go to Solution.
2019-07-08 5:03 AM
Sure, I can try that.
I am at 4MHz right now, and I can vary from 125kHz up to 8MHz....
2019-07-09 4:21 AM
I tested from 125kHz up to 8MHz.
Except from the transfer speed, I could not identify any differences or abnormalities.
I used a Saleae Logic Pro 8 Analyzer which was able to detect and analyze the transfer at every configuation.
However, the problems at the STM32 stayed the same.
At some random point it looses a packet or some bits; which finally messes up the whole upcoming transactions.
A 6kByte transfer still won't work at all.
2019-07-10 2:17 AM
Hmm. The following works reliably for me copy-free at 12 MBit/s on two Nucleo STM32F042K6 boards (transmit master + receive slave) with STM32CubeMX generated code skeleton:
Transmitter:
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_WritePin( LD3_GPIO_Port, LD3_Pin, GPIO_PIN_SET );
HAL_StatusTypeDef status = HAL_SPI_Transmit_DMA( &hspi1, buffer, len );
if( status != HAL_OK ) {
Error_Handler();
}
HAL_GPIO_WritePin( LD3_GPIO_Port, LD3_Pin, GPIO_PIN_RESET );
HAL_Delay(100);
}
Receiver:
char buffer[512*8];
int i=1;
volatile int done = 0;
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
HAL_StatusTypeDef status = HAL_SPI_Receive_DMA( &hspi1, buffer+i*512, 512 );
i++;
if(i==8) {
i=0;
done = 1;
}
}
and in main():
HAL_StatusTypeDef status = HAL_SPI_Receive_DMA( &hspi1, buffer, 512 ); // very first DMA
for(;;) {
if(done) {
HAL_UART_Transmit( &huart2, buffer, sizeof(buffer), HAL_MAX_DELAY );
done=0;
}
}
Frank
2019-07-15 5:03 AM
Now, from this code I understood how to implement the "pointer-shifting" for DMA ( buffer+i*512 ), thanks.
I updated my code now and got rid of the copying parts. Thus, my received data will be written in the frame_buffer immideately.
That works so far, but still does not solve the main problem that the devices hangs up.
@Frank Bauernoeppel: Is your setup still working if you increase the data amount? Up to e.g. 10, 12 or even 20 packets á 512 Byte?
The code you presented is sending 4096 Byte per transaction. At my setup that works for roughly 50 transaction till the systems hangy up.
As closer as I go towards the 6000 Bytes per transfer, the system hangs up earlier and earlier.