2020-07-16 1:28 AM
Hello everyone,
I have designed a board with STM32F750N8, 22 Bit Parallel Nor Flash, 13 Bit SDRAM, QSPI Nor Flash.
Now i am trying to read, write data, read device id from fmc nor flash (other memories not enabled). But when i try to read device id, getting 0x90 as Manufacturer Code, 0x2FC as Dev Code 1, 2, 3.
When i read back what i wrote, i am getting 0xF0 as first word (16bit), 0x2FC as rest of the 4096 word (16bit).
I think nor flash works but somehow there is a problem and cause this. What am i missing? I coppied STM32756G_EVAL FMC Nor example. Even timings.
I have attached my nor flash schematic, cubemx project, some codes.
I used MT28EW128ABA1HPC-0SIT flash memory IC.
What am i missing? Why 0x02FC is everywhere?
NOT: I am using internal RC oscillator with 216 MHz.
Here is FMC Init function with msp and mpu init:
/* FMC initialization function */
static void MX_FMC_Init(void)
{
FMC_NORSRAM_TimingTypeDef Timing = {0};
/** Perform the NOR1 memory initialization sequence */
/* Timing */
Timing.CLKDivision = 2;
Timing.DataLatency = 2;
Timing.DataSetupTime = 8;
Timing.AddressHoldTime = 3;
Timing.AddressSetupTime = 4;
Timing.BusTurnAroundDuration = 1;
Timing.AccessMode = FMC_ACCESS_MODE_A;
/* hnor1.Init */
hnor1.Instance = FMC_NORSRAM_DEVICE;
hnor1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
hnor1.Init.PageSize = FMC_PAGE_SIZE_NONE;
hnor1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;
hnor1.Init.NSBank = FMC_NORSRAM_BANK1;
hnor1.Init.MemoryType = FMC_MEMORY_TYPE_NOR;
hnor1.Init.WaitSignal = FMC_WAIT_SIGNAL_ENABLE;
hnor1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
hnor1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
hnor1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hnor1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hnor1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hnor1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hnor1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_ENABLE;
hnor1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
hnor1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
hnor1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ASYNC;
/* ExtTiming */
if (HAL_NOR_Init(&hnor1, &Timing, NULL) != HAL_OK)
{
Error_Handler( );
}
}
static void HAL_FMC_MspInit(void){
GPIO_InitTypeDef GPIO_InitStruct ={0};
if (FMC_Initialized) {
return;
}
FMC_Initialized = 1;
/* Peripheral clock enable */
__HAL_RCC_FMC_CLK_ENABLE();
/** FMC GPIO Configuration
PE4 ------> FMC_A20
PE3 ------> FMC_A19
PD7 ------> FMC_NE1
PE5 ------> FMC_A21
PD6 ------> FMC_NWAIT
PD0 ------> FMC_D2
PD5 ------> FMC_NWE
PD1 ------> FMC_D3
PF0 ------> FMC_A0
PD4 ------> FMC_NOE
PF1 ------> FMC_A1
PF2 ------> FMC_A2
PF3 ------> FMC_A3
PF4 ------> FMC_A4
PF5 ------> FMC_A5
PD15 ------> FMC_D1
PD10 ------> FMC_D15
PD14 ------> FMC_D0
PD9 ------> FMC_D14
PD8 ------> FMC_D13
PF12 ------> FMC_A6
PG1 ------> FMC_A11
PF15 ------> FMC_A9
PD12 ------> FMC_A17
PD13 ------> FMC_A18
PG3 ------> FMC_A13
PG2 ------> FMC_A12
PF13 ------> FMC_A7
PG0 ------> FMC_A10
PE8 ------> FMC_D5
PD11 ------> FMC_A16
PG5 ------> FMC_A15
PG4 ------> FMC_A14
PF14 ------> FMC_A8
PE9 ------> FMC_D6
PE11 ------> FMC_D8
PE14 ------> FMC_D11
PE7 ------> FMC_D4
PE10 ------> FMC_D7
PE12 ------> FMC_D9
PE15 ------> FMC_D12
PE13 ------> FMC_D10
*/
// GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Pin = FMC_A20_Pin|FMC_A19_Pin|FMC_A21_Pin|FMC_D5_Pin
|FMC_D6_Pin|FMC_D8_Pin|FMC_D11_Pin|FMC_D4_Pin
|FMC_D7_Pin|FMC_D9_Pin|FMC_D12_Pin|FMC_D10_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = FMC_NE_Pin|FMC_NWAIT_Pin|FMC_D2_Pin|FMC_NWE_Pin
|FMC_D3_Pin|FMC_NOE_Pin|FMC_D1_Pin|FMC_D15_Pin
|FMC_D0_Pin|FMC_D14_Pin|FMC_D13_Pin|FMC_A17_Pin
|FMC_A18_Pin|FMC_A16_Pin;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
GPIO_InitStruct.Pin = FMC_A0_Pin|FMC_A1_Pin|FMC_A2_Pin|FMC_A3_Pin
|FMC_A4_Pin|FMC_A5_Pin|FMC_A6_Pin|FMC_A9_Pin
|FMC_A7_Pin|FMC_A8_Pin;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
GPIO_InitStruct.Pin = FMC_A11_Pin|FMC_A13_Pin|FMC_A12_Pin|FMC_A10_Pin
|FMC_A15_Pin|FMC_A14_Pin;
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
}
/**
* @brief Configure the MPU attributes as as device for NOR.
* @note The Base Address is 0x60000000.
* The Region Size is 16MBytes, it is related to NOR memory size.
* @param None
* @retval None
*/
static void MPU_ConfigNOR(void)
{
MPU_Region_InitTypeDef MPU_InitStruct;
/* Disable the MPU */
HAL_MPU_Disable();
/* Configure the MPU attributes as WT for SRAM */
// MPU_InitStruct.SubRegionDisable = 0x00;
// MPU_InitStruct.BaseAddress = 0x68000000;
// MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
// MPU_InitStruct.Enable = MPU_REGION_ENABLE;
// MPU_InitStruct.Number = MPU_REGION_NUMBER1;
// MPU_InitStruct.Size = MPU_REGION_SIZE_8MB;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
/* Configure the MPU attributes as device for NOR */
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.BaseAddress = 0x60000000;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.Size = MPU_REGION_SIZE_16MB;
// MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
// MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
// MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
// MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
// MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enable the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
//And here is my main function:
int main(void)
{
/* USER CODE BEGIN 1 */
/* Set MPU NOR region */
MPU_ConfigNOR();
/* Enable the CPU Cache */
// CPU_CACHE_Enable();
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_FMC_Init();
/* USER CODE BEGIN 2 */
// BSP_NOR_Init();
/* Read NOR memory ID */
if(HAL_NOR_Read_ID(&hnor1, &NOR_Id) != HAL_OK)
{
/* NOR read ID Error */
Error_Handler();
}
/* Test the NOR ID correctness */
if( (NOR_Id.Manufacturer_Code != (uint16_t)MANUFACTURER_CODE) ||
(NOR_Id.Device_Code1 != (uint16_t)DEVICE_CODE1) ||
(NOR_Id.Device_Code2 != (uint16_t)DEVICE_CODE2) ||
(NOR_Id.Device_Code3 != (uint16_t)DEVICE_CODE3))
{
/* NOR ID not correct */
Error_Handler();
}
/* Return to read mode */
BSP_NOR_ReturnToReadMode();
/* Fill the buffer to write */
Fill_Buffer(aTxBuffer, BUFFER_SIZE, 0x2323);
/* Erase block */
BSP_NOR_Erase_Block(WRITE_READ_ADDR);
/* Write data to the NOR memory */
for (uwIndex = 0; uwIndex < BUFFER_SIZE; uwIndex++)
{
/* Write data to NOR */
HAL_NOR_Program(&hnor1, (uint32_t *)(NOR_BANK_ADDR + WRITE_READ_ADDR + 2*uwIndex), &aTxBuffer[uwIndex]);
/* Read NOR device status */
if(HAL_NOR_GetStatus(&hnor1, NOR_BANK_ADDR, PROGRAM_TIMEOUT) != HAL_NOR_STATUS_SUCCESS)
{
return HAL_NOR_STATUS_ERROR;
}
}
/* Read back data from the NOR memory */
if(HAL_NOR_ReadBuffer(&hnor1, NOR_BANK_ADDR + WRITE_READ_ADDR, &aRxBuffer[0], BUFFER_SIZE) != HAL_OK)
{
return HAL_ERROR;
}
uwWriteReadStatus = Buffercmp(aTxBuffer, aRxBuffer, BUFFER_SIZE);
if (uwWriteReadStatus != PASSED)
{
while(1)
{
}
}
while (1)
{
}
}
2020-07-17 12:20 AM
No body have any idea?