cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4cube examples - but where ?

M G_2
Associate III
Posted on June 27, 2018 at 16:17

Dear Community,

I’ve just installed the STM32F4cube from SetupSTM32CubeMX-4.26.0.exe  but I cannot find the “

Hundreds of examples for easy understanding

� mentioned on

https://www.st.com/en/embedded-software/stm32cubef4.html

  or in AN4739.

Unfortunately the installer hasn’t installed a folder having a similar name

like STM32Cube_FW_F4_VX.Y.Z\Projects\. .

I would be very glad if someone could give a hint how to also instal those examples.

1 ACCEPTED SOLUTION

Accepted Solutions
Posted on June 27, 2018 at 17:12

Go into the settings from CubeMX and look where you put the repository

E:\CT\STM32Cube\Repository\STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Applications\FatFs\FatFs_USBDisk

0690X0000060PHdQAM.jpg

This is Help -> Updater Settings

If you haven't installed the F4 packages, install those

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2
Posted on June 27, 2018 at 17:12

Go into the settings from CubeMX and look where you put the repository

E:\CT\STM32Cube\Repository\STM32Cube_FW_F4_V1.0\Projects\STM32F4-Discovery\Applications\FatFs\FatFs_USBDisk

0690X0000060PHdQAM.jpg

This is Help -> Updater Settings

If you haven't installed the F4 packages, install those

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 27, 2018 at 22:11

Dear Clive,

the repository folder mentioned in your post is there but without any software in it. I’ve followed your hint to also download the F4cube “en.stm32cubef4.zip� and viola it contained all the examples I was searching for. Thank you very much for your help.