cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F466RE: How many clock cycles to access data sram memory?

kag_embedded
Associate

For application benchmarking, I would like to access the data memory of the STM32F466RE in a single cycle.
What is the data load latency of the STM32F466RE from data SRAM at 84MHz?

and, if it is not single cycle, can I reduce the core frequency to decrease the number of SRAM access cycles?

Thank you.

1 REPLY 1
AScha.3
Chief II

see ds:

AScha3_0-1728071757650.png

 

If you feel a post has answered your question, please click "Accept as Solution".