STM32F446RE CAN in LOOPBACK MODE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-09 7:45 PM
Hello Everyone,
I want to test the CAN1 peripheral in loop back mode. please suggest me the required steps .
I am using STM32F446RE nucleo board and currently i want to test without transceivers
So far i have done this .
/* CAN1 init function */
static void MX_CAN1_Init(void){hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 16; hcan1.Init.Mode = CAN_MODE_LOOPBACK; hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ; hcan1.Init.TimeSeg1 = CAN_BS1_1TQ; hcan1.Init.TimeSeg2 = CAN_BS2_1TQ; hcan1.Init.TimeTriggeredMode = DISABLE; hcan1.Init.AutoBusOff = ENABLE; hcan1.Init.AutoWakeUp = DISABLE; hcan1.Init.AutoRetransmission = DISABLE; hcan1.Init.ReceiveFifoLocked = DISABLE; hcan1.Init.TransmitFifoPriority = DISABLE; if (HAL_CAN_Init(&hcan1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
/*♯♯-2- Configure the CAN Filter ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
sFilterConfig.FilterBank = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.SlaveStartFilterBank = 14; if(HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK) { /* Filter configuration Error */ Error_Handler(); }uint8_t aData[]= {0xA5,0X55};
uint8_t RxData[8]; CAN_TxHeaderTypeDef tXheader; CAN_RxHeaderTypeDef RxHeader; tXheader.StdId = 0x11; tXheader.ExtId = 0; tXheader.IDE = CAN_ID_STD; tXheader.RTR = CAN_RTR_DATA; tXheader.TransmitGlobalTime = DISABLE; tXheader.DLC = 2; HAL_StatusTypeDef Status; /*♯♯-3- Start the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ if (HAL_CAN_Start(&hcan1) != HAL_OK) { /* Start Error */ Error_Handler(); } Status = HAL_CAN_AddTxMessage(&hcan1,&tXheader,aData,&TxMailbox); if(Status != HAL_OK) { Error_Handler(); } /* Wait transmission complete */ while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan1) != 3) {} /*♯♯-5- Start the Reception process ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ if(HAL_CAN_GetRxFifoFillLevel(&hcan1, CAN_RX_FIFO0) != 1) { /* Reception Missing */ Error_Handler(); }Start the Reception process : This function is entering in to error_handler .
Could you please help to solve this issue ?
Thank you !
#can-interface #stm32f4xx-can-bus-error #stm32- Labels:
-
CAN
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-16 7:35 AM
Hi
balckiran
‌,In the package STM32CubeF4 package, you find a ready to use example for CAN in loopback mode with STM32F446 device.
It is underSTM32Cube_FW_F4_V1.0\Projects\STM32446E_EVAL\Examples\CAN\CAN_Loopback.
You find there a readme.txt file that describes how to run the example.
Compare the one I provided with your generated project and add same APIs calls to check again.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-18 2:07 AM
Amel,
Thanks for the help, yes i indeed referred to the code you mentioned but the problem is the transmission is not successful , i debugged the IRQ and the control is going to TERR ( Transmission error). Actually i am using silent loop back without any transceiver.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-18 2:45 AM
If you don't have a transceiver, then you need a pull-up on Can-Rx.processor pin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-18 3:17 AM
ok,
then you need to purchase a Commercial CanBus testing unit, like CanDo from the UK.
I set the CanDo unit to transmit packets every second.
I worked on the receiver first.
This requires a transceiver chip and a 120ohm terminator if your wires are over 10Meters.
it is impossible to debug your code from here.
but this looks odd. if(HAL_CAN_GetRxFifoFillLevel(&hcan1, CAN_RX_FIFO0) != 1)
char canFifo1FullFlag = CAN1->RF1R & CAN_RF1R_FMP1;
if (canFifo1FullFlag) {
{
readCanBytecount = (CAN1->sFIFOMailBox[1].RDTR & 0x0f);
canRxMsgBottomWord[canRxMsgIN] = CAN1->sFIFOMailBox[1].RDLR; // load all eight bytes in 2 cycles
canRxMsgTopWord [canRxMsgIN] = CAN1->sFIFOMailBox[1].RDHR;
canRxMsgID[canRxMsgIN] = CAN1->sFIFOMailBox[1].RIR >> 21;
CAN1->RF1R |= CAN_RF1R_RFOM1; // release FIFO
canRxMsgLength[canRxMsgIN] = readCanBytecount; // was 0x10+ to signify FIFO1
++canRxMsgIN &= 0x3F; // 64 entries only
canRxMsgTableEMPTY = false;
if (canRxMsgIN == canRxMsgOUT) canRxMsgTableFULL = true;
}
CAN1->IER |= CAN_IER_FMPIE1; // (11) Set FIFO1 message pending IT enable
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-18 3:58 AM
yes . i do have pull up on RX. i connected to +vcc via 3.3K resistor