cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-C092RC Demo Program: Loopback L1(L) -> L3 ==> FAILED

SSimm.6
Associate II

I have a NUCLEO-C092RC board.  When I connect to a terminal and start the board I get:

 Demo mode launch
test sw version SW V-0.2.0
- Loopback L1(L) -> L3 ==> FAILED

I have looked around and haven't found what the 'failure' is.  I would also like to see the code for the demo (haven't found that either).  I would assume that I just don't where to look.

 

Regards & thanks...

11 REPLIES 11
mƎALLEm
ST Employee

Hello,


@SSimm.6 wrote:

 Demo mode launch
test sw version SW V-0.2.0
- Loopback L1(L) -> L3 ==> FAILED
..


Where you get that Error message? is that possible to share a screenshot of this error?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks for the prompt reply.  This is the output from the virtual COM port on the NUCLEO board after a reset.  It might be a while before I am able to respond to other queries.  Regards.

test sw version SW V-0.2.0
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L1(L) -> L3 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED
- Loopback L3(L) -> L1 ==> FAILED

Demo mode launch

 

Hello,

Still not clear from where this error message comes from?

Is it from an existing example? if Yes which one?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
SSimm.6
Associate II

This is what is loaded on the NUCLEO-C092RC ( assume this is the Demo Program from the factory ).  When I attach to the board (I have 2) and attach to the virtual com port that is what I get on boot/reset.  I get the same results.

Ok clear.

Moved to the Embedded Software forum board as the question is related to the board demo.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
SSimm.6
Associate II

Where is that forum?  Link?

Thanks


@SSimm.6 wrote:

Where is that forum?  Link?

Thanks


I've already moved the post. You are in the correct forum board now.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I can't find post on the forums. I don't see an Embedded Software forum.

 


@SSimm.6 wrote:

I can't find post on the forums. I don't see an Embedded Software forum.

 


Your post is already in the "STM32 Embedded Software" forum board:

mALLEm_0-1743160122260.png

PS: unfortunately I don't have the NUCLEO board to test the behavior.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.