2017-03-16 6:59 PM
2017-03-17 8:04 AM
Hi
GB_H_Pin GA_L_Pin GA_H_Pin GC_L_Pin GC_H_Pin GB_L_Pin
GA_H_GPIO_Port GC_L_GPIO_Port
are looking special.
Was it generated with CubeMX?
The names do not match for one member each.
Dieter
2017-03-17 9:37 AM
,
,
Hi,
Yes, I generated the initial code with CubeMX. I've since then modified the timer initialization functions to what I previously tested on the Nucleo. The names are defined in main.h and shown below.
♯ define
GC_L_Pin GPIO_PIN_7♯ define
GC_L_GPIO_Port GPIOC♯ define
GC_L TIM_CHANNEL_2♯ define
GC_H_Pin GPIO_PIN_8♯ define
GC_H_GPIO_Port GPIOC♯ define
GC_H TIM_CHANNEL_3♯ define
GB_L_Pin GPIO_PIN_9♯ define
GB_L_GPIO_Port GPIOC♯ define
GB_L TIM_CHANNEL_4♯ define
GB_H_Pin GPIO_PIN_9♯ define
GB_H_GPIO_Port GPIOA♯ define
GB_H TIM_CHANNEL_2♯ define
GA_L_Pin GPIO_PIN_10♯ define
GA_L_GPIO_Port GPIOA♯ define
GA_L TIM_CHANNEL_3♯ define
GA_H_Pin GPIO_PIN_11♯ define
GA_H_GPIO_Port GPIOA♯ define
GA_H TIM_CHANNEL_42017-03-17 10:35 AM
In an old code, the PWM generation was setup like this:
void SetTimerOutputCC_SingleEdge(Timer_t* Timer, u32 n, u32 Value_lsb) { Timer->EdgesSize[n] = 0; // Non zero triggers the DMA mode for multiple pulses Timer->EdgesTableAdr[n] = 0;TIM_OCInitTypeDef OC;
TIM_OCStructInit(&OC); OC.TIM_OCMode = TIM_OCMode_PWM2; OC.TIM_OutputState = TIM_OutputState_Enable; OC.TIM_Pulse = Value_lsb; OC.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OCnInit(Timer->TIM, n, &OC);}Or when starting the code, after enabling the timer clock, force a
__HAL_RCC_TIM1_FORCE_RESET();
__HAL_RCC_TIM1_RELEASE_RESET();
This should make the peripheral closer to the HW Power on reset.
Or the PWM depends on the initial pin level?
2017-03-17 3:27 PM
TIM_OC_InitTypeDef
sConfigOC;
[...]
sConfigOC.
OCMode
= TIM_OCMODE_PWM1;sConfigOC.
Pulse
= 10;sConfigOC.
OCPolarity
= TIM_OCPOLARITY_HIGH;sConfigOC.
OCFastMode
= TIM_OCFAST_DISABLE;
if
(HAL_TIM_PWM_ConfigChannel(&htim, &sConfigOC, TIM_CHANNEL_2)You have to have initialized *all* members of
TIM_OC_InitTypeDef struct before calling HAL_TIM_PWM_ConfigChannel. This for Advanced timers (i.e. TIM1 and TIM8) among others includes the polarity of the inverted output. You surely already know this from the concise and detailed 'library' manual.
JW
2017-03-18 1:06 PM
I tried the force reset and release to no success. In fact, it made it so channels 2 & 3 were always inverted instead of randomly inverting.
2017-03-18 1:09 PM
Well, that did it! The CubeMX code has the inverted output config calls as well, but I deleted them since I didn't have them during my testing. Thank you!
This is the code that works:
sConfigOC.
OCMode
= TIM_OCMODE_PWM1;sConfigOC.
Pulse
= 100;sConfigOC.
OCPolarity
= TIM_OCPOLARITY_HIGH;sConfigOC.
OCNPolarity
= TIM_OCNPOLARITY_HIGH;sConfigOC.
OCFastMode
= TIM_OCFAST_DISABLE;sConfigOC.
OCIdleState
= TIM_OCIDLESTATE_RESET;sConfigOC.
OCNIdleState
= TIM_OCNIDLESTATE_RESET;2017-04-06 8:30 PM
I had the exactly same problem as OP, and I fixed the problem too. OCNPolarity was problem. I only missed that field in the previous code.