2017-03-30 09:47 AM
I see varying information about whether the timers in my STM32F437 are 16 bit or 32. Maybe I missed a table in RM0090 or the data sheet. Could someone please point me to a place where this info might be consolidated?
So far by hit or miss it seems TIM2 is 32 bits and TIM4 is 16?
Thanks,
JH
Solved! Go to Solution.
2017-03-30 11:55 AM
Oh yes, and Table 6 in the DS, DocID024244 Rev 10, might provide some insight, too...
JW
2017-03-30 09:49 AM
RM0090 deals with this, although not in a single place, you have to read the introduction of all 4 timer chapters.
But, if you believe me, only TIM2 and TIM5 are 32-bit, the rest is 16 bit.
JW
2017-03-30 11:55 AM
Oh yes, and Table 6 in the DS, DocID024244 Rev 10, might provide some insight, too...
JW
2017-03-30 12:08 PM
Thanks, JW. I will take your word for it.
2017-03-30 02:57 PM
TIM2 and TIM5, pretty sad for a 32-bit micro, a small part of me weeps that someone in the design meeting didn't say *NO* much louder!!
'Up to 17 timers: up to twelve 16-bit and two 32- bit timers up to 180 MHz, each with up to 4 IC/OC/PWM or pulse counter and quadrature (incremental) encoder input'
12+2 is 14, even for extremely large values of 2, and you can't count the 32-bit ones twice. And I'm pretty sure both the 32-bit timers on APB1 at 45 MHz (TIMCLK 90 MHz)
Who needs 17 timers anyway? Kind of indicative you've got some sub-par ideas about how a singular timer needs to function. How about ONE timer with 17x 32-bit comparators, or THREE with 8x?
2017-03-30 03:44 PM
12+2 is 14, even for extremely large values of 2
They count up the RTC, and the two watchdog *timers* - said Table 6 does not show this anymore, but you can see it in other STM32 DS. Funnily, SysTick is not counted.
How about ONE timer with 17x 32-bit comparators, or THREE with 8x?
Fancy to start ''2017 Easter WishList''? ;-)
Jan