2018-12-10 5:37 AM
Hi everyone!! I am from Taiwan
I am currently working on a project that records time using STM32F429IIT6
VBAT is connected to the 3.3V output of the power supply.
PDR_ON is connected to VDD
Power on when VDD is powered off
Time will be initialized
Project output is with STM32CUBE
I really don't know what to do.
please help me
2018-12-10 7:52 AM
What are the symptoms?
What is the initialization code of RTC?
Did you try to look at some of the example projects related to RTC?
JW
2018-12-11 7:07 AM
Hi JW
I am trying to print out the value of RTC_BKP_DR0
The value of the first RTC_BKP_DR0 is 0X32F2
Later I changed the value of RTC_BKP_DR0 to 0X1111
Download to the STM32F429IIT6
After NRST is triggered, RTC_BKP_DR0 is still 0X32F2
But after I cut off VDD, I will re-power it. The value of RTC_BKP_DR0 is 0X1111
VBAT has connected to Super capacitor
I don't know if this is normal
RTC_BKP_DR0 should still be 0X32F2, it should not be 0x1111
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.