2017-08-03 1:55 PM
Hi guys, total newb question here: A few weeks back I got a STM32F429. Immediately when I received it, I plugged it in and played with the demo software which seemed to work fine. Busy with other things, I stored it away safely for the last few weeks.
Just today I go to work with it, plug it back in and all I get is a white LCD screen, the COM LED is flashing periodically and the power LED is continuously on as shown in the image below.
Despite having the ST-Link/V2 drivers installed, Windows does not acknowledge the board as a plugged in USB device.
Searching this forum and Google have not provided me with any leads. Anyone have any ideas?
Solved! Go to Solution.
2017-08-06 3:46 AM
Hello!
Check if your USB cable fits properly to the socket, and/or change the cable
Check the Black button (reset) if has stucked
Check Idd jumper for proper fitting.
With a multimeter, check VDD pin , The voltage must be around 3v
2017-08-05 8:17 PM
Bump
2017-08-06 3:46 AM
Hello!
Check if your USB cable fits properly to the socket, and/or change the cable
Check the Black button (reset) if has stucked
Check Idd jumper for proper fitting.
With a multimeter, check VDD pin , The voltage must be around 3v
2017-08-06 3:48 PM
My bad, looks like a USB cable that although physically fits perfectly is not working with this board and another I had. I must've gotten the cable mixed up in between using it previously and now. Thanks so much. Sorry for the bother.
2017-10-25 4:37 AM
Hey!
It's great that you've solved your problem. But I suggest you to perform a firmware update as well. This update will eliminate issues when powering the board from the 5V pin. This update is extremely beneficial when powering the board from a battery.
Cheers!
2017-10-25 6:58 AM
Thanks! Will do!
2019-03-27 10:04 AM
Hey Friend ! Were you able to solve the problem ? Because changing the cable didn't worked for me.
2019-03-28 5:03 AM
Yeah, I believe the problem is that some USB cables are just for charging and not also communicate data(?) I had mistakenly used one of these cables.
2019-03-28 8:21 AM
@Terence D I have almost the same problem as your's .
Here's the link to my thread : https://community.st.com/s/feed/0D50X0000AaXYvU
Can you help me with any suggestions? Any help will be appreciable.
2019-03-28 7:34 PM
Yes, I am quite sure this was the problem I had: https://electronics.stackexchange.com/questions/140225/how-can-i-tell-charge-only-usb-cables-from-usb-data-cables