STM32F429 NAND conflict withSDRAM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-21 12:55 AM
I have a board based on the stm32f429. There is a 16M Bytes SDRAM (MT48LC16M8) and a 32M bytes NAND (NAND128W3A2B) connected to the FMC bus.
I used one area of the SDRAM as the LTCD buffer,such as: /* Start Address configuration : the LCD Frame buffer is defined on SDRAM */ LTDC_Layer_InitStruct.LTDC_CFBStartAdress = LCD_FRAME_BUFFER; There is two strange problem: [1] The nand write/read is always unstable, sometimes went wrong. After months of trying, I finally found that: The nand operation is ok if I turn off the LTDC controller, namely not using the SDRAM as frame buffer. the command is: LTDC_Cmd(ENABLE); [2] Even I turn off the LTDC controller, if I use the upper 8M bytes of sdram, the nand still generates write error. To summarize: The only working nand operation is to satisfy both: a. Turn off the LCD controller; b. configure the SDRAM as using 8M bytes only: FMC_SDRAMInitStructure.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_9b; FMC_SDRAMInitStructure.FMC_RowBitsNumber = FMC_RowBits_Number_12b; If I configure to use the whole 16M SDRAM like: FMC_SDRAMInitStructure.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_10b; FMC_SDRAMInitStructure.FMC_RowBitsNumber = FMC_RowBits_Number_12b; nand will go wrong. I have researching this problem for months, can't find the answer, could anyone help me out. Even a hint maybe will help me find the solution. Thank you very much! If I only use the- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-21 1:07 AM
What Address bits does the NAND use to differentiate between the command/data interfaces? What timing/stability requirements does the NAND have wrt the data and address buses?
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-21 1:13 AM
Both nand and sdram are 8 bits.
For Nand, i mm using the wait feature, the configuration is:p.FMC_SetupTime = 0x1;
p.FMC_WaitSetupTime = 0x3; p.FMC_HoldSetupTime = 0x2; p.FMC_HiZSetupTime = 0x1;FMC_NANDInitStructure.FMC_Bank = FMC_Bank2_NAND;
FMC_NANDInitStructure.FMC_Waitfeature = FMC_Waitfeature_Enable; FMC_NANDInitStructure.FMC_MemoryDataWidth = FMC_NAND_MemoryDataWidth_8b; FMC_NANDInitStructure.FMC_ECC = FMC_ECC_Disable; FMC_NANDInitStructure.FMC_ECCPageSize = FMC_ECCPageSize_512Bytes; FMC_NANDInitStructure.FMC_TCLRSetupTime = 0x00; FMC_NANDInitStructure.FMC_TARSetupTime = 0x00;- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-21 1:23 AM
Could this problem be related to that one ? FMC on F429 has an errata.
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy.st.com%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32F429%20FMC%20SDRAM%20problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&cur...- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-21 2:07 AM
> Could this problem be related to that one ? FMC on F429 has an errata.
+1
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy.st.com%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32F429%20Silicon%20Revision%203%20ETA&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506... JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-21 5:38 AM
I am not sure if I understanding this errota correctly, does this mean:
SDRAM and NAND cannot be used at the same time in some chip production version?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-22 12:46 AM
Could anyone explain what does this workaround means regarding to the ''FMC dynamic and static bank switching''
Description The dynamic and static banks cannot be accessed concurently. Workaround Do not use dynamic and static banks at the same time. The SDRAM device must be in self-refresh before switching to the static memory mapped on the Nor or NAND controller. Before switching from static memory to SDRAM, issue a normal command to wake-up the device from self-refres mode. Does my situation means ''concurrently access'': reading/wring from NAND while the LTDC using SDRAM as framebuffer. The nand is using BANK 2, the SDRAM is using bank 5.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-22 1:38 AM
Unfortunately, yes. The errata means, that to use NAND, you need to stop using SDRAM, and vice versa.
JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-22 2:23 AM
That doesn't make sense, because I can read/write nand directly to a SDRAM area if turn off the LTDC controller. Like:
u8 pcDest[0x100000] __attribute__((at(0xc0200000))); uffs_read(fd, pcDest, header.ulFileSize);- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-18 6:06 AM