cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 Disc1 LED5 (Vbus pin is working)

jonathanmeyer
Associate II

Hello guys, 

I have an issue that when I program the board, LED5(it says Vbus LED) is lighting. (it is green) Datasheet of the board hasn't got a info or i cant see any info about that.

Could you help me with this issue ? Thank you...

2 REPLIES 2
TDK
Guru

What exactly is the issue? It is lit up and you don't want it to be? Or don't think it should be?

Look at the schematic to see how LD5 is wired up.

https://www.st.com/en/evaluation-tools/32f429idiscovery.html#cad-resources

 

If you feel a post has answered your question, please click "Accept as Solution".
KDJEM.1
ST Employee

Hello @jonathanmeyer ,

-> "Datasheet of the board hasn't got a info or i cant see any info about that."

What do you mean the datasheet of the board. Could you please share the document link ?

It is mentioned in the  UM1670 User manual Discovery kit with STM32F429ZI MCU that "LD5: The green LED indicates when VBUS is present on CN6 and is connected to PB13 of the STM32F429ZIT6".

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.