cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F413VGT I2C1 Support 1MHz?

GYUYEONLEE
Associate II

According to Datasheet, I2C of STM32F413VGT can be increased to 1 MHz, is it possible?

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

@GYUYEONLEE wrote:

i2c.png

 

 So DS11581 Rev 7 / page 35.

They can reach 1MHz but not fully Fast mode Plus compliant. The fast mode needs 20 mA output current drive for Fast-mode Plus operation.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
TDK
Super User

You just asked this, and it was answered:

https://community.st.com/t5/stm32-mcus-products/stm32f413vgt-i2c-support-fast-mode-plus-1mhz/td-p/883847

FMPI2C can do 1 MHz. I2Cx cannot.

Please don't repost.

If you feel a post has answered your question, please click "Accept as Solution".

If you look at Datasheet, I'm asking because there's a phrase that says you can raise it up to 1mHz. I've checked that it's divided into FMPI2C and I2C, but I'm asking because there's a phrase that I2C can also increase to 1MHz.

 

Hello,

When you refer to the documentation in a post you need definitely to provide the document reference (DSxxx / revision) + the page and preferably a screenshot of that statement.

Thank you

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

i2c.png

 

Here is In Datasheet. In datasheet I can see increased up to 1MHz.


@GYUYEONLEE wrote:

i2c.png

 

 So DS11581 Rev 7 / page 35.

They can reach 1MHz but not fully Fast mode Plus compliant. The fast mode needs 20 mA output current drive for Fast-mode Plus operation.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.