2024-01-09 12:05 PM
Good Evening Ladies and Gentlemen,
A short introducing purpose of mine:
int main(void)
{
RCC->AHB1ENR |= 0xFC; // ---> Here I would like to open the Port clock
RCC->APB1ENR |= 0xFC; // ---> Here I would like to open the USART2 clock - in this context not relevant
GPIOA->MODER |= 0x55555555; // ---> Here I define Port A as output
GPIOC->MODER |= 0x55555555; // ---> Here I define Port C as output
GPIOA->ODR |= (1<<2); // ---> Here I would like to set PA2 "high"
GPIOC->ODR |= (1<<13); // ---> Here I would like to set the onboard LED (PC13) "high"
while(1) {
GPIOA->ODR |= (1<<0); // Here I would like to "toggle" PA0 and PA6
GPIOA->ODR |= (1<<6);
delayMs(50); // It only is a not relevant "delay" for this purpose
GPIOA->ODR &= ~(1<<0);
GPIOA->ODR &= ~(1<<6);
delayMs(50);
}
}
But something went wrong - it does not work - Do you have any suggestions especially regarding a simple "toggling"?
It should be a pre work for a stepper motor controlling.
Best regards
~TIMBO~
2024-01-11 11:58 AM - edited 2024-01-11 11:58 AM
RMW is an abbreviation (acronym) from Read-Modify-Write.
For example, if you write
GPIOA->ODR |= (1<<0);
that is a Read-Modify-Write operation, because:
- first, the processor reads in content of GPIOA->ODR register into some of its internal working registers
- then the processor performs the bitwise-OR operation with (1 << 0), that's the modify part
- and finally, processor writes from internal register into GPIOA->ODR the modified value
JW
2024-01-11 1:21 PM
And that is only possible with a BSRR register?
2024-01-11 1:33 PM
In spite of it - I would like to set A2 and A6 as "high" - and toggle with the ODR register A0.
Could you write shortly the mode register setting, too?
2024-01-12 1:52 AM
Don't use "A0" etc. It's PA0, PA2 and PA6. "A0" may cause confusion with Arduino-connector signal marking.
For PA0 to be set as output, you have to set bits 0 and 1 of GPIOA_MODER to 0b01.
For PA2 to be set as output, you have to set bits 4 and 5 of GPIOA_MODER to 0b01.
For PA6 to be set as output, you have to set bits 12 and 13 of GPIOA_MODER to 0b01.
You may see a pattern and write macros/functions accordingly.
I recommend to try it without writing any program (maybe an infinite loop), by directly writing to registers in the debugger.
Then, to set pin PA0 high, write 1 into bit 0 of GPIOA_BSRR. This has to be a direct write, not a RMW with OR:
GPIOA->BSRR = (1 << 0);
To set pin PA2 high, write 1 into bit 2 of GPIOA_BSRR:
GPIOA->BSRR = (1 << 2);
To set pin PA6 high, write 1 into bit 6 of GPIOA_BSRR:
GPIOA->BSRR = (1 << 6);
To set pin PA0 to low, write 1 into bit 16 of GPIOA_BSRR:
GPIOA->BSRR = (1 << (0 + 16));
To set pin PA2 to low, write 1 into bit 18 of GPIOA_BSRR:
GPIOA->BSRR = (1 << (2 + 16));
To set pin PA6 to low, write 1 into bit 22 of GPIOA_BSRR:
GPIOA->BSRR = (1 << (6 + 16));
You may have spotted a pattern here, too; again, try to write a macro or a function.
You may want to read this intro.
JW
2024-01-12 10:22 AM - edited 2024-01-12 11:13 AM
RCC->AHB1ENR |= (1<<0)|(1<<2); // enable A and C port
RCC->APB1ENR |= (1<<17); // enable USART2
GPIOA->MODER |= (1<<0)|(1<<4)|(1<<12); // set A0, A2, A6 as output
GPIOC->MODER |= (1<<26); // set PC13 as output
GPIOA->BSRR = (1 << 2);
GPIOA->BSRR = (1 << 6);
GPIOC->BSRR = (1 << (13 + 16));
while (1)
{
GPIOA->BSRR = (1 << 0);
delayMs(50);
GPIOA->BSRR = (1 << (0 + 16));
delayMs(50);
}
Thank you for your answer.
Result:
PC13 is glowing
PA0 "toggled" - but the stepper motor does not drive... thank you in spite of it ...
2024-01-12 11:32 AM - edited 2024-01-12 11:32 AM