2023-03-15 1:20 AM
Hi i wanted to try new extension but i get this error. The code is a basic blink its working on cubeide but when i try on vscode this happens.
Thank you already
[build] c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: cannot open linker script file C:/newcodes/ledblink/STM32F407VGTX_FLASH.ld: No such file or directory
[build] collect2.exe: error: ld returned 1 exit status
2023-03-15 1:46 AM
Hi @Hüseyin Avni Sarıkaya
Did you check that the path is valid? Or, if the file is missing, you can try to copy it from the original project.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-15 1:52 AM
Yeah path is valid and file is missing but i didnt try copiying it is linker files project spesific or its global for that mcu?
2023-03-16 7:24 AM
could you try a shorter path please without special characters
2023-03-23 4:32 PM
If the linker file is missing how is this building in STM32IDE? Did you import this project using the STM32 extension in VSCode?