2013-12-05 3:17 AM
Hey there,
Our problem is that we get random faults (memory, bus or usage)! The handlers are calling sporadically between 10s to some hours! But we have also pcb�s without any issues! We are using a custom environment with a STM32F405ZGT and an external PSRAM! From software side we have the Keil os without micro lib (due to usage of a cpp library) We are using excessive dynamic memory but only in external RAM! All other RAM access goes to internal one. A further interface we are using in a high priority is the SPI2 interface with DMA functionality! If we stop in an error handler, we recognize invalid addresses in pc (like: 0xE0C001E0; 0x804AED2; 0xFFFFFFFE; 0x46604630 or 0x00000000) Does anybody have an idea? #stm32f4 #stm32 #fault2014-01-06 7:44 AM