STM32f4 Timer1 counting pulses
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-11 2:34 AM
Hello all,
I want to count pulses with TIMER 1, because he has the fastest counting frequency.
I was able to count pulses with TIMER 2 but something in my code is missing to make it work for Timer 1: (I also checked the reference manual ...)
Maybe someone knows something that I missed.
Here is my Code:
void timer_1_pulse_counter_gpioa1_Init(void){
RCC->AHB1ENR |= 0x01; // 1: IO port A clock enabled
//RCC->AHB1ENR |= 0x10; // 1: IO port E clock enabled
// APB1 peripheral reset register
RCC->APB2ENR |= 0x01; // 1: enable TIM2
// GPIO port mode register (GPIOx_MODER)
GPIOA->MODER |= 0x00000008; // 10: Alternate function mode PA1 => AF mode
GPIOA->AFR[0] |= 0x00000010; // 1000: (alternate function for TIM1/ TIm2)
GPIOA->PUPDR |= 0x00000008; // Sets pull down resistor for PA1
// CCMR!: capture/compare mode register 1
TIM1->CCMR1 |= 0x0200; // CC2 ... , IC2 is mapped on TI1
TIM1->SMCR |= 0x0007; // Bits[2:0] 111: External Clock Mode 1 - Rising edges of the selected trigger clock the counter.
TIM1->SMCR |= 0x0050; // Bits[6:4] 110: selected Trigger: Filtered Timer Input 1 (TI1FP1)
// 0x0050
TIM1->ARR = 0xFFFF; // Set the timer reset on the highest possible value
TIM1->CR1 |= 0x0001; //0001 Enable Timer
}
- Labels:
-
STM32F4 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-11 11:40 AM
Which STM32f4 ?
PA1 has no TIM1 functionality. See Alternate function mapping table in datasheet.
Assuming you have a pin mapped to TIM1_CH2 in GPIO:
> TIM1->CCMR1 |= 0x0200; // CC2 ... , IC2 is mapped on TI1
This would enable TIM1_CH1 rather than TIM1_CH2; it's not what you want.
And with TIM1_CH2 you would need to select TI2FP2 in TIMx_SMCR.TS.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 10:45 AM
Hey Jan,
thanks for your answer.
I own a STM32f407 board. I found this mapping table in the reference manual on side 272 (https://www.st.com/resource/en/reference_manual/dm00031020-stm32f405-415-stm32f407-417-stm32f427-437-and-stm32f429-439-advanced-arm-based-32-bit-mcus-stmicroelectronics.pdf ).
For me it seems like PA1 has a TIM1 functionality. Did I made here a mistake ?
(I change then to TIM1_CH2 and TI2FP2 in TIMx_SMCR.TS )
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 11:11 AM
That's just a general drawing. The interconnection matrix is sparse. See the table in datasheet I referred to above.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 11:16 AM
Ah know I got it. This is just a general reference manual. So I found the table in the Datasheet of stm32f407!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-13 8:29 AM
Hey Jan,
I configured now everything for TIM8 (works for be better, because I have an additional board).
But somehow the counting is not working: I use PC6 in AF3 TIM8_CH1.
Do you have a suggestion for me ?
My Code:
RCC->AHB1ENR |= 0x04; // 1: IO port C clock enabled
//RCC->AHB1ENR |= 0x10; // 1: IO port E clock enabled
// APB1 peripheral reset register
RCC->APB2ENR |= 0x01; // 1: enable TIM1
// GPIO port mode register (GPIOx_MODER)
GPIOC->MODER |= 0x2000; // 10: Alternate function mode PC6 => AF mode
GPIOC->AFR[0] |= 0x3000000; // 1000: Must refer to AF3 (alternate function for TIM8)
GPIOC->PUPDR |= 0x2000; // Sets pull down resistor for PA1
// CCMR!: capture/compare mode register 1
TIM8->CCMR1 |= 0x01; // CC1 channel is configured as input, IC1 is mapped on TI1
// 0x0100
TIM8->SMCR |= 0x0007; // Bits[2:0] 111: External Clock Mode 1 - Rising edges of the selected trigger clock the counter.
TIM8->SMCR |= 0x0050; // Bits[6:4] 110: selected Trigger: Filtered Timer Input 1 (TI1FP1)
// 0x0050
TIM8->ARR = 0xFFFF; // Set the timer reset on the highest possible value
TIM8->CR1 |= 0x0001; //0001 Enable Timer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-13 8:38 AM
> RCC->APB2ENR |= 0x01; // 1: enable TIM1
Didn't you say TIM8?
Using symbols from the CMSIS-mandated device header reduces this risk.
RCC->APB2ENR |= RCC_APB2ENR_TIM8EN;
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-14 1:02 AM
Somehow it is still not working.. Do you have another suggestion ?
void timer_8_pulse_counter_gpioa1_Init(void){
RCC->AHB1ENR |= 0x04; // 1: IO port C clock enabled
//RCC->AHB1ENR |= 0x10; // 1: IO port E clock enabled
// APB1 peripheral reset register
RCC->APB2ENR |= RCC_APB2ENR_TIM8EN; // 1: enable TIM8
// GPIO port mode register (GPIOx_MODER)
GPIOC->MODER |= 0x2000; // 10: Alternate function mode PC6 => AF mode
GPIOC->AFR[0] |= 0x3000000; // 1000: Must refer to AF3 (alternate function for TIM8)
GPIOC->PUPDR |= 0x2000; // Sets pull down resistor for PA1
// CCMR!: capture/compare mode register 1
TIM8->CCMR1 |= 0x01; // CC1 channel is configured as input, IC1 is mapped on TI1
// 0x0100
TIM8->SMCR |= 0x0007; // Bits[2:0] 111: External Clock Mode 1 - Rising edges of the selected trigger clock the counter.
TIM8->SMCR |= 0x0050; // Bits[6:4] 110: selected Trigger: Filtered Timer Input 1 (TI1FP1)
// 0x0050
TIM8->ARR = 0xFFFF; // Set the timer reset on the highest possible value
TIM8->CR1 |= 0x0001; //0001 Enable Timer
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-14 9:28 AM
I tried now another board and now it is working. Maybe something was broken on my old board. But still, thanks for your help!!