2024-05-23 3:35 AM
Hello Team,
I am using the STM32F469NIH6 to implement a timer triggered DMA and I need some clarity on a few points here-
I see that that there are three possible requests possible for a timer triggered DMA. I understand that the TIM8_UP is to trigger a DMA request with an update event (which occurs when the counter overflows/underflows)
What is the TIM8_CH4/TRIG/COM all about? How is it different from the TIM8_CH1 request? Any leads on this would be of help !
Thank you,
Janani Sunil
2024-05-23 8:46 AM
> TIM8_CH1 request
That's triggered by a Capture or Compare event on TIM8_CH1, if TIM8_DIER.CC1DE is set.
> TIM8_CH4/TRIG/COM
That's triggered by one of the Capture/Compare on TIM8_CH4, or the Trigger event (i.e. edge of TRGI signal as selected by TIM8_SMCR.TS), or the Commutation event (that is a rarely used event I am not going to discuss here); again, if respective DMA-enable bit is set in TIM8_DIER.
JW
2024-05-23 11:14 PM - edited 2024-05-23 11:15 PM
Hi @waclawek.jan ,
Thank you for your response.
I am trying to operate timer 8 in ETR Mode (in slave trigger mode) and I have enabled TIM8_CH1 DMA request for the same (Master TRGO OC mode). I am supplying an external PWM signal to the respective ETR pin allocated for timer 8.
Upon configuring this, when I probe the ETR pin, I see that my master signal that I apply is getting corrupted.
Am I missing out on any configuration here?
Thank you,
Janani
2024-05-24 1:30 AM
> when I probe the ETR pin
Which pin is that?
> I see that my master signal that I apply is getting corrupted.
What hardware is this, your own, or some "known good" board like Nucleo or Disco?
Read out and check/post content of timer and relevant GPIO registers.
JW
2024-05-24 3:25 AM - edited 2024-05-24 3:25 AM
PA0 is the ETR pin that I am using for TIM8_CH1
I am using the SDP-K1, which has an STM32F469NIH6 mounted on it.
The timers and the GPIOs seem to be configured right.
Thank you again for your inputs.
Regards,
Janani
2024-05-24 4:22 AM
> The timers and the GPIOs seem to be configured right.
Yet you complain about a timer-related pin working strangely.
How else do you propose to debug it? The mcu works out of its registers, not out of source code or CubeMX clicks.
JW