2014-05-22 7:59 AM
Our application will use FreeRTOS for the OS. We are using the STM32F4-Discovery eval board in our alpha unit. The development environment is Keil MDK-ARM Professional/ uVision 5.
I need an example to understand how to use FreeRTOS with this processor with Keil MDK-ARM. I have used STM32CubeMX to generate code with FreeRTOS included, however, I need an example to understand where and how to put my tasks in the user areas. Are there any examples illustrating a simple 2 task FreeRTOS application? I get this up and running easily using Keil and RTX, but we must use FreeRTOS. #stm32f4-freertos #example-code2014-05-28 2:50 AM
Hi
Have you checked the FreeRTOS download web page? http://www.freertos.org/a00090.html#ST There is a demo fro STM32F405 but it is for IAR. The next nearest match is a NXP LPC4350 demo using Keil/RVDS The descriptions of the demo make them sound complicated. It may be easier to look at the demos, how they statically create tasks and write your own 2 task demo to learn how to do it.2014-05-28 11:26 AM
Hi sung.chen_chung,
I finally figured this out by mapping the Keil two task Blinky example in RTX to the FreeRTOS code generated using STM32CubeMX. I did not realize, until attending an STmicro seminar last week, that you must put added code in the delineated /* USER AREAS */ or reinvoking CubeMX on the project would overwrite your code.. Thanks