2014-03-10 06:34 PM
LD8 LED is ON (USB over-current) regardless to program. Furthermore receiving data by UART3 using pin PC11 is impossible, but with PD9 works fine. Earlier
I had no
problems
, and now
after connected the
board
to the computer
is something wrong. Please tell me what can cause problems. Thank you2014-03-11 01:24 AM
- Did you bring any hardware update to the board?
- EarlierI had no
problems
Do you mean before connecting USB? Could you share minimum helpful code to understand issue? (May be you forgot to enable clock) -MaylaTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-03-11 11:56 AM
I have worked on the program, that received data from UART3 and sended it by USB OTG to PC. It worked fine for a few weeks. Before the last connection to PC by CN1, when I saw, that pin PC11 was damaged (reception don't work) and LD8 is on, I had updated the ST-Link firmware to 2.19. After update I worked with my board for some hours. When I connected the Discovery to PC next day, there was problem described above.
I think this is hardware problem (not in my code), because LD8 lights even if I clean flash memory using STM32 ST-Link Utility, but maybe there is some solution?