2012-07-05 10:45 AM
friends i ported the code of ''STM324xG-EVAL'' to stm32f4 discovery....and i made it work almost completely....bt some errors are coming on output...
i am posting two images regarding this..problem 1: problem 2: and also attatching my code keil....urgent help needed #!telegraphing2012-07-07 11:26 PM
hey buddy thanks for your help dude...i made it working....i just change that 25MHz to 8Mhz...nd some little settings...nd now rtc is working fine....so guys i made rtc workin super fine...
thanks @clive2012-07-08 2:06 AM
hey brother... my rtc worked properly for the first two or three times...bt now again RTC prescalar config failed is coming ...i dont know why it is happening with me,,, so what should i check for this and one more thing no signal is coming from 8Mhz oscillator...i checked that on pin PH0 & PH1......plz help me..