2015-11-17 1:49 AM
Hello there,
I am working on an application now where I have to be able to reprogram the chip memory from a connected PC (most likelly USB). I have read that there are BOOT0 and BOOT1 lines which allows one to jump to the hardware serial bootloader (I am not sure if USB works too?). The problem is I wont be able to phisically short/ pull them by only having usb connection. I was wondering, can I set the BOOT1/0 registers by software, so I can restart the mcu and boot it into hardware bootloader only by using USB connection?2015-11-17 2:41 AM
Hi Bremen,
In order to be able to reprogram the chip memory from a connected PC, I recommend you review the example STM32Cube_FW_F4_V1.9.0\Projects\STM324xG_EVAL\Applications\USB_Device\DFU_Standalone. It describes how to use USB device application based on the Device Firmware Upgrade (DFU) on the STM32F4xx devices.As recommended in the readme file, the DFU demo can be downloaded fromhttp://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1533/PF257916
.It is possible to bypass the BOOT pins and use software configuration to select the memory accessible at address 0x00000000: you have to use SYSCFG_MEMRMP for this purpose (Refer to RM0090).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-11-17 2:49 AM
Thank you :).
2015-11-17 4:47 AM