cancel
Showing results for 
Search instead for 
Did you mean: 

SPI, I2C

arunl4g
Associate II
Posted on November 17, 2015 at 11:41

Hey, 

i have a stm32f407 board .

Can anyone tell me whats the best way  or possible ways to test the i2c and spi driver. 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on November 17, 2015 at 14:54

Hi m.dums,

You can do some tests based on the examples that you may find in STM32CubeF4 package or F4 standard library.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

arunl4g
Associate II
Posted on November 17, 2015 at 15:00

what i mean is that, i dont have device that connected with  spi or i2c interface. so i would like to know, is there any device that i can buy and test the driver ? or is there any solution other that connecting two boards ?

Posted on November 17, 2015 at 15:10

Isn't there a MEMS and CODEC devices you can talk too on the board? Use those. 

Failing that get yourself some I2C or SPI FLASH/EEPROM devices and talk to those.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..