2014-12-08 9:18 AM
Hi
I am still (trying to learn) learning how to code STM32F devices using Keil MDK and maybe foolishly, made a pcb with a STM32F383CC6 on it.Firstly how do I use the Keil MDK or CubeMX when it does not appear to recognise STM32F383xx?Secondly, why is it a 383 when it is has a M4 core?Thanks for any clues.Kind regardsDerek #stm32f3782014-12-08 10:31 AM
You'd probably talk to your Keil support contact and get an appropriate patch, or pick a STM32F3 part which is adequately similar to build your project. Outside the peripheral view in the debugger this is of little import.
The STM32F1 has an Cortex-M3, all the STM32F3 parts have a Cortex-M4F, I'm not sure there's a way to try and rationalize the part# to core#, it's just an exercise that will give you a headache. Not a lot of data on the STM32F383, what drew you to the part, and wouldn't it have been easier to have started tinkering with a DISCO board?2014-12-09 1:42 AM
Hello Derek,
STM32F383 samples where renamed later ''STM32F378''.So using Keil or CubeMX, you have to select this part number.STM32F378 is similar to STM32F373 (with mainly the 16-bit sigma-delta ADCs)but it operates at 1.8 V +/-8% to be supplied by an external voltage regulator.More details on the STM32F378CC are available on this page: http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1576/LN1838/PF259874.Best Regards,-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-12-09 2:30 AM
Thanks both Mayla and Clive1
I only picked it because of foot print size and Farnell stocked it. They appear to do both the 383 and the 378?? Many thanks for the explanation Kind regards derek