2013-11-20 1:57 AM
For a project in which I have to measure temperature as well, I would like to run the SDADC continuously but with a slower clock than 500kHz. Concerning the datasheet 500kHz is the minimum. Is there a explanation for this value, or can I go underneath? What do I have to expect when I will run it with 100kHz?