2014-02-28 4:53 PM
hello,
i'm trying to set up PDE0-1-2-3-4-5 for external interrupt. I want to have 6 pin near each other just to have a nicer cabling layout. I set up the clock, the pin as input. Then i have to set up SYSCFG_EXTILineConfig() for every pin, right? Then i set up EXTI_Init() with EXTI_LineX, where X goes from 0 to 5, because every pin is in a different line (reference manual page 190) Then i have to set up NVIC_Init(), i use EXTI0_IRQn, but is it only about priority and to group interrupt?, or there is HW related, like for line? i'm a bit confused. also, now i'll have to write a void EXTI0_IRQHandler(void), with have to pay attention on witch pin generate the interrupt, or there is alredy somenthing that does that for me? thank you. #stm32f3-interrupt-discovery2014-02-28 7:17 PM
You'll set up ONE pin per EXTI Line#, and set up the multiple interrupts (NVIC/Handler) they will be directed too. EXTI Line#5 thru #9 going to EXTI9_5_IRQHandler
EXTI0_IRQHandler ; EXTI Line0 EXTI1_IRQHandler ; EXTI Line1 EXTI2_TS_IRQHandler ; EXTI Line2 and Touch EXTI3_IRQHandler ; EXTI Line3 EXTI4_IRQHandler ; EXTI Line4 EXTI9_5_IRQHandler ; External Line[9:5]s See also STM32F3-Discovery_FW_V1.1.0\Project\Peripheral_Examples\EXTI_Example2014-03-01 6:16 AM
Thank you very much! DS was not really clear, and because ''multiuple'' EXT_IRQ wasn's near other EXT_IRQ, i missed them.
found out the the IRQ 10-15 is perferct for me, as i want to READ 6 asinc PPM signal. that's my code, hope it is right and will help someone (nb: micros() is a function that return number of us from the board start up, i don't care about overflow as it is an unsigned int 32, so the subtraction math will always be correct)/*
thanks to clive1
*/
uint32_t high_start[] = { 0, 0, 0, 0, 0, 0 };
volatile uint32_t ppm_value[] = { 0, 0, 0, 0, 0, 0 };
void
external_interrupt_init() {
GPIO_InitTypeDef GPIO_InitStructure;
EXTI_InitTypeDef EXTI_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the pin Clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
//or TIM
int
i = 0;
for
(i = 0; i < 6; i++) {
/* Configure pin as input */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = 1<<(i+10);
GPIO_Init(GPIOE, &GPIO_InitStructure);
/* Connect Button EXTI Line to GPIO Pin */
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOE, i + 10);
/* Configure EXTI line */
EXTI_InitStructure.EXTI_Line = i + 10;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
}
/* Enable and set EXTI Interrupt with the lowest priority */
NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
void
EXTI15_10_IRQHandler(
void
) {
int
i;
for
(i = 0; i < 6; i++) {
if
(EXTI_GetITStatus(i + 10) == SET){
//IF pin is now HIGH
if
(high_start[i] == 0){
//and no read as started
high_start[i] = micros();
//nail it as HIGH signal start
}
}
else
{
//IF pin is now LOW
if
(high_start[i] != 0){
//and just before there was HIGH signal
ppm_value[i] = micros() - high_start[i];
//calculate PPM value (should be between ~1000us and ~1800us)
high_start[i] = 0;
//prepare for the next reading
}
}
EXTI_ClearITPendingBit(i+10);
//clear pending interrupt
}
}