cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303 CubeMX injected conversion of ADC rank 2 do not work

l.kopp
Associate II

Hi,

I'm using the STM32F303 and CubeMX with low layer.

I try to read two ADC-values with the injected conversion. In CubeMX i defined two ranks to read the values from the ADC. For rank 1 everything works fine and in the JSQ1 register contains the right channel. For rank two i'd like to read channel 1 but in the JSQ2 register channel 0 is selected.

Have anyone a solution for this problem ?

Thanks, L.

0 REPLIES 0