Hi,I'm using the STM32F303 and CubeMX with low layer.I try to read two ADC-values with the injected conversion. In CubeMX i defined two ranks to read the values from the ADC. For rank 1 everything works fine and in the JSQ1 register contains the righ...
Hello everybody,i have a motor control application and try to trigger a ADC in injected conversion mode with the Output Compare (OC4REF) trigger of TIM1. With my configuration the ADC convert only once and then never reach the HAL_ADCEx_InjectedConvC...
Hello,I try to trigger a ADC for example ADC1 in injected conversion mode with the Timer out event of TIM1 but it doesn`t work. For Time 1 i select OCREF and OC6REF as trigger event. In my ADC I select the Timer 1 Trigger out event as external trigge...
Hey everybody,I updated CubeMX to Version 5.2 and now I miss the NVIC initialisation, for example for my TIM1 interrupt.Do anybody know how I can fix this problem ?Best regards
Yes I use this to build two different Project Targets with different versions of the HAL Drivers. Each Target have a own Output Folder and even wehen I delete alle .o-Files in the folder this message occures.