cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f302 usart interrupt problem

lijieamd
Associate
Posted on April 01, 2015 at 03:31

Hi all, I configure my stm32f302's usart without peripheral lib, when i enable it with CR1->UE, the usart interrupt keep triggered and CR1->UEbit cleared automatically, actually i didn't connect anything to RX and TX pin.

My code here:


void
USART1_IRQHandler(
void
)

{

Uart_gp_slave_uart_event(&uart_gp_slave);

}


void
Uart_gp_slave_uart_event(
struct
_s_uart_gp_slave *uart)

{

uint32_t isr = uart->UART->ISR;


uart->UART->ICR = LITERAL_BIN32(00000000,00010010,00011011,01011111);


if
( isr & USART_ISR_TC )

{

RO_DMA_CLR_ISR(uart->DMA, uart->DMA_TX_CH_INDEX);

uart->DMA_TX_CH->CCR &= ~DMA_CCR_EN;

uart->state = UART_GP_SLAVE_TX_IDLE;

}

if
( isr & USART_ISR_IDLE )

{

RO_DMA_CLR_ISR(uart->DMA, uart->DMA_RX_CH_INDEX);

uart->rx_done_callback(uart->rxLength - uart->DMA_RX_CH->CNDTR);

uart->DMA_RX_CH->CCR &= ~DMA_CCR_EN;

uart->DMA_RX_CH->CNDTR = uart->rxLength;

uart->DMA_RX_CH->CCR |= DMA_CCR_EN;

}

}


void
Uart_gp_slave_abstract_ini(
struct
_s_uart_gp_slave *uart)

{

NVIC_InitTypeDef NVIC_InitStruct;


//GPIO ini

Ro_gpio_setup( uart->GPIO_TX, uart->GPIO_TX_Pin,

RO_GPIO_MODE_AF, RO_GPIO_OUT_PP, RO_GPIO_SP_HIGH, RO_GPIO_PULL_NO);

Ro_gpio_setup( uart->GPIO_RX, uart->GPIO_RX_Pin,

RO_GPIO_MODE_AF, RO_GPIO_OUT_PP, RO_GPIO_SP_HIGH, RO_GPIO_PULL_NO);

Ro_gpio_setup( uart->GPIO_DE, uart->GPIO_DE_Pin,

RO_GPIO_MODE_AF, RO_GPIO_OUT_PP, RO_GPIO_SP_HIGH, RO_GPIO_PULL_NO);


Ro_gpio_af_setup(uart->GPIO_TX, uart->GPIO_TX_Pin, uart->GPIO_AF_TX);

Ro_gpio_af_setup(uart->GPIO_RX, uart->GPIO_RX_Pin, uart->GPIO_AF_RX);

Ro_gpio_af_setup(uart->GPIO_DE, uart->GPIO_DE_Pin, uart->GPIO_AF_DE);


//UART ini

uart->UART->CR1 = LITERAL_BIN32(00000011,11111111,00000000,01011100);

uart->UART->CR2 = LITERAL_BIN32(00000000,00000000,00000000,00000000);

uart->UART->CR3 = LITERAL_BIN32(00000000,00000000,01000000,11000001);


uart->UART->BRR = 0x12; 
// 4MBps


//DMA ini

uart->DMA_TX_CH->CCR = LITERAL_BIN32(00000000,00000000,00000000,10011000);

uart->DMA_TX_CH->CPAR = (uint32_t)(&(uart->UART->TDR));


uart->DMA_RX_CH->CCR = LITERAL_BIN32(00000000,00000000,00000000,10001000);

uart->DMA_RX_CH->CPAR = (uint32_t)(&(uart->UART->RDR));


// UART interrupt

NVIC_InitStruct.NVIC_IRQChannel = uart->UART_IRQ;

NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 1;

NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStruct);


uart->UART->CR1 |= USART_CR1_UE;

}

#usart #stm32f3 #stm32
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on April 01, 2015 at 06:34

You look to enable the Idle interrupt.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
lijieamd
Associate
Posted on April 01, 2015 at 07:26

thanks for your reply, clive1.

yes, i want to use idle interrupt to detect rx frame end

but i think idle interrupt would not keep trigger when rx is idle because i had used stm32f4's usart idle interrupt before, it just triggered one time after one frame